List of Contributions

Steve Wehr

Contact Details

Steve Wehr


My Content

1 to 13 of 13 total
Posted By Steve Wehr Feb 20, 2026 06:40:10 AM
Found In Egroup: Advanced Software
\ view thread
Thanks Baldrick -------------------------------------------
Posted By Steve Wehr Feb 19, 2026 12:21:00 PM
Found In Egroup: Advanced Software
\ view thread
Has anyone tried to use the wizard in the Edge and connect to Micro800? The MicroController driver is not listed when using the wizard. Do I need to update firmware? -------------------------------------------
Posted By Steve Wehr Dec 13, 2024 07:58:00 AM
Found In Egroup: Advanced Software
\ view thread
I there a native printing feature for Alarms in Optix? I need to print alarms as they occur to a single line printer.
Posted By Steve Wehr Nov 11, 2024 01:43:00 PM
Found In Egroup: Advanced Software
\ view thread
I have a project where I would like to run a power point based on product and location selection from PV and PLC. PPT file would be located on network drive. Has anyone done anything similar? Is it possible to run a power point within Optix and have it run slide show to the end and repeat? or Would I ...
Posted By Steve Wehr Oct 08, 2024 06:55:00 AM
Found In Egroup: Advanced Software
\ view thread
AutomateShane, Recently Rockwell has release Faceplates(FP) for Optix that can be used with Rockwells Power Monitor 5000, I was trying to get them connected using ethernet/IP. I can not find any documentation or instructions for the faceplates on how to connect them within Optix. I have the manual for ...
Posted By Steve Wehr Oct 07, 2024 03:24:00 PM
Found In Egroup: Advanced Software
\ view thread
I am trying to connect a PM5000 to the FTOptix FP. Do I need to have a PLC or can I do a direct connection in Optix? Any help appreciated.
Posted By Steve Wehr Aug 09, 2023 06:00:00 AM
Found In Egroup: Advanced Software
\ view thread
AutomateShane I figured it out. I had to go to the the option gear at top right and select "Factory talk Optis Studio options" then select "Advanced Mode". Now when I right click on objects with variables I see "Refactor". One last thing though, it did not automatically create Displayed value ...
Posted By Steve Wehr Aug 08, 2023 05:19:00 PM
Found In Egroup: Advanced Software
\ view thread
AutomateShane This is what I see with right click on object with two variables. I updated to Beta version 1.3.0.310 to see if I would get the refactor in the list and it is the same as version 1.2. Any ideas why you have it in your selection and I do not? I am using pro version.
Posted By Steve Wehr Aug 07, 2023 03:59:00 PM
Found In Egroup: Advanced Software
\ view thread
Where do I find refactor, I can not find either refactor or Transform Instance into type.
Posted By Steve Wehr Aug 07, 2023 01:37:00 PM
Found In Egroup: Advanced Software
\ view thread
AutomateShane I created object(Productconfig)with two variables, then I created object(Product), my issue is that when I right click on that object(Product) I do not see option for new object types, or my previously created object(productconfig) In the list. I only see object.
Posted By Steve Wehr Aug 02, 2023 07:57:00 AM
Found In Egroup: Advanced Software
\ view thread
Automateshane, what version of Optix are you running? I have 1.2.0.263. It will not let me select object type for (Product1) and change it to my other object with variables (Productconfig). Am I missing something or might there be an issue with the version I am running?
Posted By Steve Wehr Jul 31, 2023 06:19:00 PM
Found In Egroup: Advanced Software
\ view thread
Thank You, very helpful. ------------------------------ Stick ------------------------------
Posted By Steve Wehr Jul 27, 2023 07:13:00 AM
Found In Egroup: Advanced Software
\ view thread
What is the best way to create a list selector that is similar to the one in ME?