List of Contributions

Cuong

Contact Details

Cuong


My Content

1 to 8 of 8 total
Posted By Cuong Dec 01, 2025 08:29:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Dear Support Team, I am currently using FT Optix HMI connected directly to the PM5000 using the Use Device Libraries. I would like to use the email sending functionality provided in this device library. However, I am facing an issue where the system is sending too many emails. I need to send an ...
Posted By Cuong Aug 04, 2025 11:48:18 PM
Found In Library: Advanced Software
Posted By Cuong Aug 04, 2025 11:48:00 PM
Found In Egroup: Advanced Software
\ view thread
Dear team, I have followed the instructions and configuration of Device Libraries for FTOPTIX and directly connected to PM5000. However, when I created an Alarm (Voltage Loss V1, Transient Indication, setpoint active) on the PM5000, I did not receive the notification email as shown in the video ...
Posted By Cuong May 07, 2025 04:44:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Batman, Thanks for your support. After reaching the desired speed by analog input speed (up to 2000 rpm), it will switch to running at the preset speed (PR mode or change speed register 1) without stopping. Thank you.
Posted By Cuong May 06, 2025 03:35:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Dear team, I want to control Kinetix 5100 with an analog input. At a certain speed, switch to running PR mode ( position). For example, the machine speed from 0 rpm to 2000 rpm = 4- 20mA or 0- 10V. When it reaches 2000 rpm, it will work according to PR mode. Do you have any idea for this? ...
Posted By Cuong Mar 27, 2025 11:09:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi team, I need to migrate Ultra 3000 2098-DSD-020 1 phase 220 to the new Kinetix 2198-C4015-ERS 3 phase 380 ( Kinetix 5100 or Kinetix 5300) Motor: MPL-A320P-HK22AA to MPL-B320P-MJ72AA This is an old system: Use the first 1756-M02AE to control 2 Ultra 3000 drives. ( One of ...