List of Contributions

Phil L

Contact Details

Phil L


My Content

1 to 13 of 13 total
Posted By Phil L May 29, 2026 09:27:00 PM
Found In Egroup: Automation Control
\ view thread
Ticket Number 4011491944 - ControlLogix 5590: MSG write/read error 16#00FF ext. 16#00FF MSG The ticket has been closed. The equipment has been installed.
Posted By Phil L May 28, 2026 10:24:00 PM
Found In Egroup: Automation Control
\ view thread
I agree the forum in this instance is not the idea route for a solution, but given Rockwell Technical support have not been able to resolve the issue I thought I would enquire with a wider group to see if others had an issue. My approach to resolving issues with Rockwell Products is:- Read the ...
Posted By Phil L May 27, 2026 09:41:00 PM
Found In Egroup: Automation Control
\ view thread
No. I have had no further feedback from Rockwell. If you are using an Ethernet switch and don't disconnect the cable between the switch and the L90 Ethernet swtich it appears to work fine. The L90 is fast, I was able to run the AOI in a 1mS task and achieve decent throughput to Kepserver. Running ...
Posted By Phil L May 19, 2026 08:43:00 AM
Found In Egroup: Automation Control
\ view thread
I am using Dual IP mode. All message addresses are being setup. The system typically works, the biggest concern now is the cable disconnect and reconnect on the CPU ports only. For the socket services I have written I only delete the active instance. It is as though the Delete all Sockets does ...
Posted By Phil L May 15, 2026 06:05:00 AM
Found In Egroup: Automation Control
\ view thread
I have been using some of the new ControlLogix Processors and have found their built in Ethernet Ports to be problematic. Communicating to some third-party devices using sockets and the Rockwell Modbus TCP slave add on instruction. Each ethernet port is only communicating to a single device. The sockets ...
Posted By Phil L Nov 28, 2025 01:14:00 AM
Found In Egroup: Automation Control
\ view thread
The redundancy Cross Transfer data takes up significant CPU time. Given you are using PlantPax there will be a signficant amount of data in a random fashion which is poor for redundancy. I haven't used the redundancy for years but remember there being a formula in the manual for the crosss transfer time. ...
Posted By Phil L Feb 01, 2025 07:30:00 AM
Found In Egroup: Automation Control
\ view thread
The web browser provides that information for the L8 series. You need to have it enabled within the controller.
Posted By Phil L Jan 18, 2025 02:55:00 AM
Found In Egroup: Automation Control
\ view thread
There is no such feature. With Rockwell you can have much longer rungs and therefore you are less likely to need the feature anyway. Your only alternative is to create an extra coil. I find the long rungs in Rockwell result in more readable code.
Posted By Phil L Dec 05, 2024 09:14:00 AM
Found In Egroup: Automation Control
\ view thread
The only real benefit I see is the reduced execution time. Since I only use the fast CPU's now I don't use alias, they can only be changed via a download or messing around with temporary tags.
Posted By Phil L Dec 05, 2024 08:57:00 AM
Found In Egroup: Automation Control
\ view thread
You would need to maintain the XIC->OTE to maintain the consistency. In the past I would have the alias tag reference say TAG1_Raw, for the XIC, and TAG1 for the OTE. Then if you re-assign the hardware point you just change the alias to TAG1_Raw.
Posted By Phil L Dec 05, 2024 07:50:00 AM
Found In Egroup: Automation Control
\ view thread
In the older processors alias tags used less CPU power than a direct refence tag. In a direct reference tag the CPU has to calculate offsets from the base tag, in the same way it calculates offsets into arrays, which takes time. With the new high speed CPU's (1756-L8 and alike) the CPU time becomes far ...
Posted By Phil L Oct 18, 2024 08:36:00 AM
Found In Egroup: Advanced Software
\ view thread
The update has reduced CPU usage in Version 14, although still higher than version 13. Has anyone had issues with Version 15?
Posted By Phil L Sep 23, 2024 08:59:00 AM
Found In Egroup: Advanced Software
\ view thread
I have had a similar issue when updating from 13 to 14 with a less sophisticated display. The impact seems to be different on different hardware. I have the same application running on two PC's the three year old PC with Windows 10 is ok. The brand new top end Dell Precision workstation tops out two ...