List of Contributions

Giacomini

Contact Details

Giacomini


My Content

1 to 17 of 17 total
Posted By Giacomini Mar 31, 2024 08:59:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, I'm utilizing RSLogix 5000 version 32, and I'm unsure how to conduct a search to locate all instances of "AFI," "NOP," and similar commands utilized within the logic. Can anyone help me? Thank you, and happy Easter to all. Giancarlo
Posted By Giacomini Mar 18, 2024 04:06:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, I use the above-mentioned driver for a lifting operation and I need to release the brakes when the motor is magnetized. The driver is on the Ethernet IP network and I can't find the parameter that tells me 'motor in torque' for use in the software e open the brake. Can someone help me? ...
Posted By Giacomini Feb 29, 2024 05:48:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, I have the encoder card in slot 6 but I get that the IHM is in slot 6, how can I reset and reconfigure the entire drive? thanks in advances
Posted By Giacomini Feb 15, 2024 05:18:00 AM
Found In Egroup: Automation Control
\ view thread
Dear all, i have a couple of question for you: A) I need transfer one task (safety task in the 1756-L81ES plc model) in two identical CPU . Is it possible transfer the complete task with export / import utility or I need to transfer each routine separately? B) in a safety task I saw that a data ...
Posted By Giacomini Feb 09, 2024 04:39:48 AM
Found In Egroup: Automation Control
\ view thread
hi, Sorry, I didn't clarify well. I also need to change the number of ProfiBus node network. By By
Posted By Giacomini Feb 08, 2024 01:46:00 PM
Found In Egroup: Automation Control
\ view thread
Hi, in a system with more than 80 address, the client asks me to change the IP address: 192.168.1.xxxx to 10.109.188.xxx 255.255.255.0 to 255.255.255.288 Network is mixed ethernet IP and Profibus. What is the best way to change addresses? For the Profibus section I can use pass through of ...
Posted By Giacomini Jan 24, 2024 07:27:00 PM
Found In Egroup: Automation Control
\ view thread
Hi, I'm not finding how to use the SEQ utility, and, how to prepare a user defined SEQ. Thanks for your help. By By Giancarlo
Posted By Giacomini Jan 20, 2024 10:59:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, I have a Driver model 20G11 N C 085 JA0NNNNN which is used in an application that works with -17° inclination. The motion transmission is through pinion and rack coupling. a) Can I use this drive for this type of application? b) Somebody have a configuration example to use as a trace? ...
Posted By Giacomini Jan 20, 2024 07:08:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, Everyone, I have a question about the tag's It's possible to change Tags Usage -->Local Tag mode to Usage --> Controller? I think it's easier to use all the tags registered in Usage: Controller, what do you think? Thanks for all by by Gian ------------------------------ Giacomini ...
Posted By Giacomini Jan 14, 2024 02:21:00 PM
Found In Egroup: Automation Control
\ view thread
Hi, I'm checking an application offline that I didn't prepare. To transfer data between Main Task and Safety Task, I remember, that it was mandatory to go through a bit or word read/write program. In the application I am working now, some data passes through two programs, one for reading and another ...
Posted By Giacomini Jan 12, 2024 06:11:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, I have a doubt about using the RSOUT block. I have a doubt about using the RSOUT block. Initial situation: Enable at 0 Feedback 1 and Feedback 2 both at 1 Output 1 and Output 2 both at 0 Start of operation: I set the Enable bit to 1, Feedback 1 and Feedback 2 both at 0 Output 1 and Output 2 both ...
Posted By Giacomini Jan 10, 2024 05:23:00 AM
Found In Egroup: Advanced Software
\ view thread
Good morning, In the commissioning phase the client is asking to change the initial language of the application (English) and switch to Spanish. Is there a method that avoids opening each text individually and translating from a list extracted from the original file? Thank you all EDIT: translated ...
Posted By Giacomini Jan 06, 2024 04:24:06 AM
Found In Egroup: Automation Control
\ view thread
Hi, Thanks Philip, I solved my problem. ------------------------------ Giacomini ------------------------------
Posted By Giacomini Jan 05, 2024 02:42:00 PM
Found In Egroup: Automation Control
\ view thread
Hi, In previous versions of RSLogix, I give the impression, there was an option to delete unused tags, which I can't find in this one. Can help me? Thanks and greetings to everybody ------------------------------ Giacomini ------------------------------
Posted By Giacomini Dec 22, 2023 01:19:02 PM
Found In Egroup: Advanced Software
\ view thread
Philip, Thank you so much, ------------------------------ Giacomini ------------------------------
Posted By Giacomini Dec 22, 2023 10:36:00 AM
Found In Egroup: Advanced Software
\ view thread
Thanks, for the answer, And in situation like below, where I configure elements #1 and #2 ((#1#2.Set_FaceplateAnimation)=10) && ((#1#2.Val_Ring_Participant_Count)<47) Thanks again ------------------------------ Giacomini ------------------------------
Posted By Giacomini Dec 22, 2023 06:12:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello everybody, I'm commissioning SW that I don't prepare, and don't understand the code, /*LS:0 (#2)*/ indicated below, with which the popup is called. Somebody can help me? thanks Where I can find library that explain this codes? Thanks in advance ------------------------------ Giacomini ...