List of Contributions

VILAYIL JAMES

Contact Details

VILAYIL JAMES


My Content

1 to 20 of 50+ total
Posted By VILAYIL JAMES May 15, 2025 09:49:00 PM
Found In Egroup: Automation Control
\ view thread
Today, when It was trying to download program in the PLC, I got the below error. What is it??? I was unable to download program and we didn't put this security. How to remove this security??? How to avoid someone unauthorized person manipulate the program from remote place connected ...
Posted By VILAYIL JAMES Apr 02, 2025 12:44:00 PM
Found In Egroup: Automation Control
\ view thread
Thanks.The 8th module corresponds to slot 7 when counting from slot 0. Issue resolved: The adapter connector between the 4th and 5th module terminal bases was bent. Although the system indicated a fault in the 8th module, the actual issue was a damaged connector at the 4th module's base. After replacing ...
Posted By VILAYIL JAMES Apr 01, 2025 12:19:00 PM
Found In Egroup: Automation Control
\ view thread
I am experiencing an issue with the AENTR-IB16 digital input module. In one of the RIO panels, the fourth AENTR module and its I/O modules are encountering a problem. The configuration consists of one AENTR communication module along with eight IB16 digital input modules in the rack. The issue ...
Posted By VILAYIL JAMES Jun 22, 2024 10:39:00 PM
Found In Egroup: Automation Control
\ view thread
How can I transfer a UDT description to an individual tag description within the same UDT without copying and pasting each one individually? I need to copy and paste over 1000 equipment descriptions. Is there an easier way to accomplish this? For example, I want to move the description of TS_ARR_UDT[2] ...
Posted By VILAYIL JAMES Jun 18, 2024 10:36:00 AM
Found In Egroup: Automation Control
\ view thread
The program compiles without any errors. However, when it is downloaded to the PLC, a CIP error occurs and cancels the download. Please refer to the embedded video for more details. The error picture is also included here. Please suggest a solution. No error while compile program Video: ...
Posted By VILAYIL JAMES May 19, 2024 10:41:00 PM
Found In Egroup: Automation Control
\ view thread
Hello, I have a question regarding an AOI (Add-On Instruction) that includes two parameters (Track1_YES) which need to be entered outside the AOI, as shown in the attached picture. I frequently need to update the AOI. However, when I import the updated AOI, the previous parameter values mentioned ...
Posted By VILAYIL JAMES May 19, 2024 10:18:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Fault signal also worked. Its holding register address is 41124( 41123 in prosoft). Reg count-4. ------------------------------ JINSON KURIAN VILAYIL JAMES T&C ENGINEER, RIYADH METRO ------------------------------
Posted By VILAYIL JAMES May 10, 2024 04:50:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
The issue with the reset has been resolved. However, the logic status word still needs to be checked. This information might be beneficial to others. prosoft configuration: https://youtube.com/shorts/a1q4xmcxilU?si=p3vq-1I8I4hPuONm https://youtube.com/shorts/_N02mhzLRwY ...
Posted By VILAYIL JAMES May 10, 2024 04:24:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
problem solved. https://youtube.com/shorts/a1q4xmcxilU?si=p3vq-1I8I4hPuONm https://youtube.com/shorts/_N02mhzLRwY ------------------------------ JINSON KURIAN VILAYIL JAMES T&C ENGINEER, RIYADH METRO ------------------------------
Posted By VILAYIL JAMES May 06, 2024 10:36:00 PM
Found In Egroup: Automation Control
\ view thread
I'm curious about how to incorporate an array number into an integer tag within a PLC program. For instance, I have 16 fans represented by a UDT called 'fan' in the tag table. When accessing this UDT, there are 16 arrays available. I've connected this UDT to an AOI. For arrays with even numbers, ...
Posted By VILAYIL JAMES May 06, 2024 10:20:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Could someone kindly assist me in creating a Modbus command to reset an Allen Bradley SMC Flex soft starter? Resetting the elapsed time meter involves moving value 2 to Modbus register 41010, as demonstrated in the attached video. My PLC Modbus RTU command tag for moving the value is TVRWTO1 ...
Posted By VILAYIL JAMES May 06, 2024 10:01:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Today, the panel vendor came by and demonstrated how to reset the elapsed time on the SMC Flex soft starter. They adjusted the value to 2 at the 41010 address using Modscan32 software, and I've attached the video for reference. Immediately, right after this adjustment, the elapsed time value at address ...
Posted By VILAYIL JAMES May 04, 2024 08:10:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thank you for your response. Regarding the data reading process, I've been utilizing the 16-bit 3x holding register reading method as per earlier message. However, I've noticed a discrepancy where the register for the KWH reading, which should be the 8th register or parameter, seems to be accessed at ...
Posted By VILAYIL JAMES May 03, 2024 05:41:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
1) Could you please provide the Modbus register address for parameter #10, "meter reset," as outlined in document 150-UM008 on page 83? My understanding is that when we write a value of 1 to this register, it resets the KWH meter value, and when we write a value of 2, it resets the elapsed time. I attempted ...
Posted By VILAYIL JAMES May 01, 2024 01:14:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Could you kindly assist me in locating the Modbus register addresses for the following functionalities on the Rockwell SMC-Flex soft starter? 1. Soft start general fault (common fault) alarm 2. Power consumption kWh reading reset command( meter reset) 3. Running hour reset command (totalization) ...
Posted By VILAYIL JAMES Feb 07, 2024 07:03:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
How to unblock the Spanning Treee blocked ports as per the alarm picture. It's blocked RTU port abd no communication with SCADA. I managed to configure REP and its working OK.