List of Contributions

Glen Elam

Contact Details

Glen Elam


My Content

1 to 6 of 6 total
Posted By Glen Elam Oct 21, 2022 11:04:00 AM
Found In Egroup: Networks
\ view thread
>>You said: "If I then change the address to something else, and then back again, it will always take but sometimes it is lost (default undefined) after a power cycle." >>Does this mean that sometimes it retains the IP address and communicates just fine (for an indeterminate amount of time) after a ...
Posted By Glen Elam Oct 21, 2022 10:04:00 AM
Found In Egroup: Networks
\ view thread
The program is still there, still working, no faults. Once I change the address I can go online and see the original program. And while it is not communicating the LCD still shows the static address as originally configured, and holds it after a reset. Just changing the static address wakes it up ...
Posted By Glen Elam Oct 21, 2022 09:46:00 AM
Found In Egroup: Networks
\ view thread
Thanks for your willingness to help, Ryan, The second sentence of my original post indicated it did not respond to a ping, nor an ARP either. And that is also true when connected directly with a single cable, that is until I changed the address, as mentioned. And yes, I tried different cables, it ...
Posted By Glen Elam Oct 21, 2022 09:29:00 AM
Found In Egroup: Networks
\ view thread
1. I read the release notes for v21.7 too and though I downloaded it while I was there, had not intended on flashing it. 2. No MMI installed so no such loading. Just for grins I checked the status registers and they were zeroed. 3 & 4. One of the first things I did was connect directly to Channel 1 ...
Posted By Glen Elam Oct 21, 2022 05:38:00 AM
Found In Egroup: Networks
\ view thread
Philip, Thank you very much for the courtesy of your reply. It is very much appreciated. The processor FRN (S:62) is 11.0, but not the OS FRN (S:59) which is 21.6. That said it sounds like to much of a coincidence not to be the same issue. Are you certain it was OS FRN and not the Processor FRN? ...
Posted By Glen Elam Oct 20, 2022 02:43:00 PM
Found In Egroup: Networks
\ view thread
I am essentially trying to repeat a past configuration, and am suspecting PLC NVM failure because it accepts configuration and works for several hours, then stops communicating. The brand new ML1400 won't even respond to a ping or show up in an ARP table. Not exactly confidence building. The LCD shows ...