Posted By
Field Scada
Mar 31, 2022 10:33:00 AM
Found In
Egroup:
Networks
\
view thread
I am adding existing Genius Bus data into a L73 controller using the Prosoft An-X2-Geni Gateways. 1 per network for 5 total. Using an 1756-EN2TR as the enet interface. One network can be added successfully however, when adding the rest all connections are lost. Do the connections need to be ...
|