Posted By
KEN
Mar 12, 2024 04:30:00 AM
Found In
Egroup:
Networks
\
view thread
Please refer to the attachment for the network system,1756 redundant system. DLR network, 1756IO station IO3 and IO4 are far away from other IO stations, so in IO2, IO3, IO4, the CPU should be equipped with an optical conversion module. How do I configure this module? EDIT: moved ...
|