List of Contributions

Chris Mercer

Contact Details

Chris Mercer


My Content

1 to 2 of 2 total
Posted By Chris Mercer Mar 24, 2022 03:57:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Akbar, if you assign the Digital input to the functions you require using parameters 361 to 366 then they should start and stop the drive etc. You will also be able to start and stop using EtherNet or the HIM as all Ports are enabled by default. To alter which ports can control funtions you can ...
Posted By Chris Mercer Mar 24, 2022 03:44:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi James, You do need to be aware that the 220v Motor will be exposed to the DC Bus levels of around 680 Volts minimum and possibly as high as 2000V at the motor terminals depending on motor lead length etc. There's a really great technote here... PowerFlex AC Drive running a Lower Voltage Motor On ...