Hi James, You do need to be aware that the 220v Motor will be exposed to the DC Bus levels of around 680 Volts minimum and possibly as high as 2000V at the motor terminals depending on motor lead length etc. There's a really great technote here... PowerFlex AC Drive running a Lower Voltage Motor On ...
|