List of Contributions

LUKE BUTLER

Contact Details

LUKE BUTLER


My Content

1 to 14 of 14 total
Posted By LUKE BUTLER Sep 12, 2023 12:04:00 PM
Found In Egroup: Drives, Motion Control and Low Voltage Products
\ view thread
Hi, I am using 2198-D057-ERS3 servo amplifiers and have had them running with signals passed over a private ethernet network but for some reason I am unable to view the amplifiers in a web browser when I type the IP address into the search bar. I get an error back on my web browser saying "Access Denied". ...
Posted By LUKE BUTLER Jul 12, 2023 02:42:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, Using a dual ethernet port processor I recently had to swap all of the devices from port 1 to port 2 and vice versa. At first I attempted to drag and drop devices from 1 network to the other. This caused a problem when I opened up a ladder routine as I saw that all of my tag alias addresses had ...
Posted By LUKE BUTLER Jun 13, 2023 04:18:33 AM
Found In Egroup: Automation Control
\ view thread
Hi Fuzzy, I've just tried this and it has worked perfectly. I had previously tried importing the file back into a new project in studio 5000 and other things but to no avail! I never thought to just change the file type name manually! Thanks again ------------------------------ LUKE BUTLER - ...
Posted By LUKE BUTLER Jun 13, 2023 03:56:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, I've created a program in V32 but then I have had to flash the processor firmware up to V33 and update the processor in the program to match, no problem. I have noticed that in my file path folder a new file has been created, xxxxxx.ACD_V32 File. Does anyone know if this file can be restored ...
Posted By LUKE BUTLER Sep 21, 2022 02:24:00 AM
Found In Egroup: Automation Control
\ view thread
Thanks Philip, We generally use Compact Logix controllers for our applications (5069-L306xxx etc) but I will take a look at that video, thank you.. I thought there might have been a table or list somewhere that gave a description for any system values that can be obtained from a device. However ...
Posted By LUKE BUTLER Sep 20, 2022 10:31:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Philip, Yes we are using Ethernet/IP, the Armor Blocks part No. is 1732E-IB16M12DR. The data that I would like to know if it is possible to retrieve information such as the IP address in the form of a string, power supply level healthy, integer values that represent fault codes. Any information ...
Posted By LUKE BUTLER Sep 20, 2022 08:43:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, Is there somewhere that gives a list of the available data that can be taken from an Armor Block using the GSV instruction? We currently use the Attribute "Entry Status" to obtain the connection status healthy value but am sure that there is much more available I just can't find any specific information ...
Posted By LUKE BUTLER Apr 28, 2022 08:31:00 AM
Found In Egroup: Automation Control
\ view thread
Thanks Ryan, That's great information, in future I'll look for the comms module first rather than processor. As you described, when you create a new module from the backplane the option to select an L71 then becomes available. Many thanks for clearing that up for me. Regards, Luke
Posted By LUKE BUTLER Apr 27, 2022 02:18:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Ryan, I think you have just shown me the the missing link! In my drop down of modules I couldn't see a L71, only L81E onwards (see photo), this lead me to believe that selecting an L71 wasn't possible because it was too old. I thought I might have to go down the path of possibly selecting the generic ...
Posted By LUKE BUTLER Apr 25, 2022 09:05:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Ryan, My concern is setting up the L71 in the L310ER config. I was thinking of falling back on the option of using messages if it wasn't possible to setup a P&C between the two, but ideally this would be working over P&C. I have recently setup a MSG path between a L306ERMS2 and a 1742-L552 and ...
Posted By LUKE BUTLER Apr 08, 2022 06:07:00 AM
Found In Egroup: Automation Control
\ view thread
Hi guys, I would like to create a produce and consume (P&C) path between a 5069-L310ER processor and a 1756-L71 processor. Normally when I set up a P&C path using Studio 5000 I add the module that I want to communicate with into my ethernet navigation tree from the list of available options. If its ...
Posted By LUKE BUTLER Feb 03, 2022 07:45:00 AM
Found In Egroup: Drives, Motion Control and Low Voltage Products
\ view thread
Hi Vincent, This is exactly my point, the new motor connectors that have come in the 2198-KITCON-D057-L box do not have the orange side arms on. I can't see any difference between the new motor plugs and the old ones (2198-KITCON-D057). I suspect the wrong plugs have been put in the box. We have just ...
Posted By LUKE BUTLER Feb 02, 2022 02:30:00 AM
Found In Egroup: Drives, Motion Control and Low Voltage Products
\ view thread
Hi Vincent, Yes I have now but it doesn't provide any additional information to the document I referenced in the original post from what I can see. I will be returning to site in a couple of weeks so if the machine is down I will check the plugs against the new version (-L) and post on here if I find ...
Posted By LUKE BUTLER Jan 27, 2022 02:37:00 AM
Found In Egroup: Drives, Motion Control and Low Voltage Products
\ view thread
Hello, We recently installed some Kinetic 5700 series, D057 servo's. Installation and commissioning went well but after a few days of running we had a fault which turned out to have been caused by a motor plug coming out of the socket. Apparently this is a known issue and amplifiers which are of the ...