List of Contributions

Loo

Contact Details

Loo


My Content

1 to 4 of 4 total
Posted By Loo Jun 23, 2026 08:21:19 PM
Found In Egroup: Automation Control
\ view thread
Hi Joe, v8.016 is now released in PCDC - Product Compatibility & Download Center from Rockwell Automation. Thanks, Wan Shan
Posted By Loo Jun 22, 2026 01:14:50 AM
Found In Egroup: Automation Control
\ view thread
Hi Joe, In the current PV800 firmware, string data is not supported over Modbus RTU or Modbus TCP. In the upcoming v8.016 release, string handling will be supported over Modbus TCP (Ethernet) only. Support for Modbus RTU is not included at this time. ------------------------------ Best regards, Wan ...
Posted By Loo Apr 23, 2026 09:00:08 AM
Found In Egroup: Automation Control
\ view thread
Hi Ruschel I understand that you want to add filtering (debounce) to a digital input on Micro820. The embedded IO in Micro820 has a filtering function that will debounce any noise/chattering on the wire. This can be done via the embedded I/O device configuration page in CCW. You can also do this ...
Posted By Loo Jan 08, 2026 05:41:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Hunter, The Getting Results Guide provides an overview of all features included in this initial release, along with instructions on how to use them. If a specific feature isn't documented in the guide, it typically means it is not yet supported in v1. Best regards, Wan Shan Loo Product Manager ...