List of Contributions

Philip Hamilton

Contact Details

Philip Hamilton


My Content

1 to 20 of 50+ total
Posted By Philip Hamilton Sep 10, 2026 03:55:22 PM
Found In Egroup: Networks and SecureOT
\ view thread
Here is a video from 2022 showing ACLs in Stratix
Posted By Philip Hamilton Sep 04, 2026 03:29:00 PM
Found In Egroup: Automation Control
\ view thread
Make sure the Omron is in the 1756-DNB Scanlist (check Input/Output tabs). Download that scanlist to the 1756-DNB and put the DNB in Run mode (DNB Scanlist Active).
Posted By Philip Hamilton Aug 18, 2026 11:24:12 PM
Found In Egroup: Automation Control
\ view thread
The REST API for Logix Echo is not implemented in the Logix Echo controller using an AOI, but rather it is achieved by the optional installation of the Logix Echo SDK on the Windows PC. see Appendix A
Posted By Philip Hamilton Aug 18, 2026 09:26:00 AM
Found In Egroup: Automation Control
\ view thread
That AOI is not supported in Echo because it's based upon CIP Socket Object. he CIP Socket Interface Object (Class 0x349) is not fully supported for outgoing external communications on FactoryTalk Logix Echo controllers. Because the emulation software blocks outgoing external CIP Class 3 and raw socket ...
Posted By Philip Hamilton Aug 18, 2026 08:53:07 AM
Found In Egroup: Automation Control
\ view thread
Technology Licensing Developer How-to Guides
Posted By Philip Hamilton Aug 07, 2026 08:19:16 AM
Found In Egroup: Automation Control
\ view thread
It appears the ShutDownMacro was executed by User "aabbas" from the Display "TBX_TBB". Open the Graphic Display TBX_TBB with the editor and look for a object that calls the ShutDownMacro.
Posted By Philip Hamilton Aug 06, 2026 08:43:36 AM
Found In Egroup: Automation Control
\ view thread
The controller has two asynchronous processes: The IO tree and the Logic Scan. When you add connections to the IO tree, it creates IO tags and updates those tag at the requested packet interval, RPI. Below you see the Local IO and the Hilsher IO tag. You will write logic to copy data between these tags. ...
Posted By Philip Hamilton Aug 06, 2026 08:12:22 AM
Found In Egroup: Automation Control
\ view thread
Studio5000, Logix Designer In the IO tree, right-click the EtherNet/IP port and add the ETHERNET-BRIDGE (or "ETHERNET-MODULE Generic Ethernet Module") No other hardware required
Posted By Philip Hamilton Aug 06, 2026 08:08:35 AM
Found In Egroup: Automation Control
\ view thread
"ETHERNET-MODULE Generic Ethernet Module" is available in all Logix5000 controllers firmware v16 and later. Your 1769-L30ER (firmware v20-v38) is greater than v16, has an embedded EtherNet/IP port and supports EtherNet/IP IO. A Logix5000 controller with an EtherNet/IP port can do CIP Implicit messaging ...
Posted By Philip Hamilton Aug 06, 2026 01:23:56 AM
Found In Egroup: Automation Control
\ view thread
When starting a new Logix5000 project, there will be an embedded EtherNet/IP port listed in the IO tree. Right-click, New Module,...
Posted By Philip Hamilton Aug 05, 2026 03:06:00 PM
Found In Egroup: Automation Control
\ view thread
Input Assembly = 101 with an array of 32 bytes plus 32-bit run/idle header Output Assembly = 102 with an array of 32 bytes plus 32-bit run/idle header You might have to play with the size in bytes. I added 4 bytes to both the O->T and T->O because Hilsher showed the 32-bit header both ways and typically ...
Posted By Philip Hamilton Aug 05, 2026 12:00:00 PM
Found In Egroup: Automation Control
\ view thread
For the Logix IO tree, you need to know: Path - which will include: the IP Address for the Hilsher Slot number Assembly Instance IDs Size - how many bytes Each slot has three assemblies Input - how many bytes did you configure on the Hilscher side? Does it have the 32-bit run/idle ...
Posted By Philip Hamilton Aug 05, 2026 11:46:03 AM
Found In Egroup: Automation Control
\ view thread
Allen-Bradley does not preset the Controller as an Adapter that can be owned by a 3rd party device. The Hilscher will have to be the Adapter and the Allen-Bradley controller will be the Owner. In theory, you could make Produce tags in Logix and Consume those tags in Hilscher (the Consumer is the Owner), ...
Posted By Philip Hamilton Aug 05, 2026 09:57:00 AM
Found In Egroup: Automation Control
\ view thread
Petr, Because the Hilscher card supports EtherNet/IP Slave, I would expect the CompactLogix would own the Hilscher Input/Output Assembly Instances via the IO tree and ether an EtherNet/IP Generic (you manually enter the assembly instance IDs from the Hilscher manual) or an EDS-based Add-On Profile ...
Posted By Philip Hamilton Aug 05, 2026 09:00:18 AM
Found In Egroup: Automation Control
\ view thread
First, I'd want to know what protocols are available on both systems (e.g. Allen Bradley & Siemens could do Modbus TCP, EtherNet/IP, ProfiBUS DP etc). Then, I'd want to know what kind of data, how much data, and how often to send it. Modbus TCP is not as fast as an real-time IO connection and not used ...
Posted By Philip Hamilton Jul 31, 2026 11:21:42 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
150-C60NBD SMC-3, 60A, Open type enclosure, 460V, 120/240 Control This is the SMC-3 wiring diagram of from the installation manual. With 120Vac between A1-A2 and 120Vac at IN1 & IN2, the soft start should attempt to start the motor. Motor fails to Start 150-TG001 (Based on NEC Article 430) ...
Posted By Philip Hamilton Jul 28, 2026 11:39:19 AM
Found In Egroup: Automation Control
\ view thread
Since you have v38.02 (07/2026) installed, you should have the latest AOPs. In the v34.04 and v34.05 release notes, there are some changes to the Logix Designer component which host the AOPs so I generally I think it would be good to get the latest minor revision of the Logix Designer. Having said ...
Posted By Philip Hamilton Jul 26, 2026 07:53:38 PM
Found In Egroup: Automation Control
\ view thread
Usually OEMs use exactly the same program in all the instances of a machine and the (shared) HMI just has a separate topic/shortcut for each controller. Either the controllers each have a unique IP address or they are NAT's to create a unique address (corresponding to the unique topic/shortcut. IDK why ...
Posted By Philip Hamilton Jul 26, 2026 07:31:59 PM
Found In Egroup: Automation Control
\ view thread
RM, I would try upgrading Studio5000 from 34.03 to v34.05 (or try a different PC that already has v34.05). If you look at the release notes and search for "Add-on Profile" you'll notices some changes to the AOP host (LogixDesigner) as well as the product-specific AOPs. If you just download the product-specific ...
Posted By Philip Hamilton Jul 17, 2026 08:51:44 AM
Found In Egroup: Automation Control
\ view thread
fuzzy logic, I knew it was contained in the 24-bit memory space. I assumed it was using all 24-bit. I'm interested to see the final result. Thanks for the extra effort.