List of Contributions

Philip Hamilton

Contact Details

Philip Hamilton


My Content

1 to 20 of 50+ total
Posted By Philip Hamilton Jul 17, 2026 08:51:44 AM
Found In Egroup: Automation Control
\ view thread
fuzzy logic, I knew it was contained in the 24-bit memory space. I assumed it was using all 24-bit. I'm interested to see the final result. Thanks for the extra effort.
Posted By Philip Hamilton Jul 16, 2026 03:26:49 PM
Found In Egroup: Automation Control
\ view thread
Correct!
Posted By Philip Hamilton Jul 16, 2026 01:58:11 PM
Found In Egroup: Automation Control
\ view thread
Layden, If you copy the Timer to a DINT[3], you will see the hidden data in the first DINT. The first 3 bytes (0-2)are the CST that was captured on the previous scan of the Timer instruction. The 4th byte contains the Timer status bits... e.g. EN, TT, DN. The Timer ACC logic is like this: ...
Posted By Philip Hamilton Jul 13, 2026 08:00:00 AM
Found In Egroup: Automation Control
\ view thread
Lepton Verify the projected power consumption for all the devices in the chassis as well as the field devices (loop-powered devices). You can use IAB software as pictured below.
Posted By Philip Hamilton Jul 08, 2026 01:06:00 PM
Found In Egroup: Advanced Software
\ view thread
From inspection of the VBA... MyTagINT = 0 release (MouseUp) 1 LeftClick (MouseDn) 3 RightClick (Touch and Hold) 4 DoubleClick The VBA was not intended to "fix" anything, but rather, to help identify the mouse events. The PCAP will trigger touch event and the Window driver (or touchscreen ...
Posted By Philip Hamilton Jul 08, 2026 11:35:19 AM
Found In Egroup: Advanced Software
\ view thread
Adam, Try running this GFX which has VBA to help indicate LeftClick or RightClick and etc. Use your mouse and verify RightClick on the Text object. Then try using the touchscreen to see if it has the same action. You'll need one HMI tag called "MyTagINT" for the numeric display. FTVSE VBA-R ...
Posted By Philip Hamilton Jul 08, 2026 11:25:07 AM
Found In Library: Advanced Software
Posted By Philip Hamilton Jul 08, 2026 08:27:10 AM
Found In Egroup: Advanced Software
\ view thread
Adam, Since this issue occurs when using the PCAP touchscreen it might be a multitouch issue. A simple tap on the screen is a left mouse click. If you touch and linger (touch and hold) that becomes a right click and that would explain why you are not getting the release action. The Windows touchscreen ...
Posted By Philip Hamilton Jul 07, 2026 11:47:35 PM
Found In Egroup: Advanced Software
\ view thread
Adam, Google "HMI stuck bit" and you'll see it can happen on just about any brand of HMI software. There are various causes... probably 1/2 of the time it's related to communications being overloaded or a timing issue (PLC didn't "see" the bit change because the duration was too short). If you focus ...
Posted By Philip Hamilton Jun 30, 2026 12:47:16 PM
Found In Egroup: Automation Control
\ view thread
Duplex Mismatch can and does result in very random behavior because of undetected collisions where the packet involved in the collision is not re-sent (thus that packet never shows up). Collisions can be rare and random, thus the packet involve in the collison (where the packet is just dropped) seem ...
Posted By Philip Hamilton Jun 30, 2026 09:04:06 AM
Found In Egroup: Automation Control
\ view thread
Check for a duplex mismatch.... e.g. one end of the ethernet cable is 100 MB half duplex and the other is 100 MB full duplex
Posted By Philip Hamilton Jun 24, 2026 10:06:00 AM
Found In Egroup: Automation Control
\ view thread
I'd suggest calling tech support and have them review it. They will need to know the firmware revisions for your L7 redundancy and the Diagnostic file from both the Primary and the Secondary (RM2 module). If you want to review it yourself.... Export Diagnostics from both the Primary and the Secondary.... ...
Posted By Philip Hamilton Jun 13, 2026 07:45:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
In Logix, the External Access should be R/W... Other that that, anything external... the HMI, another Logix controller, or an Emerson controller... can R/W. Must be something on the Emerson side. What is the Output Mode in that table?
Posted By Philip Hamilton Jun 12, 2026 08:44:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Generally DeltaV will initiate R/W commands (UCMM) and Logix will respond. This is similar to how an HMI will initiate R/W commands and Logix will respond. For an HMI, a lot of the data is scatter tags. For controller to controller (Emerson to Rockwell) we generally create datasets. The easiest is to ...
Posted By Philip Hamilton Jun 11, 2026 09:17:00 AM
Found In Egroup: Advanced Software
\ view thread
Some of the advantages of #2 Historical data Store and forward - so you don't lose any data when the internet is down. Exception - In data historians (like FT Historian, OSIsoft PI or AVEVA Historian), the "swinging door" algorithm reduces storage needs. It filters out data points ...
Posted By Philip Hamilton Jun 09, 2026 06:09:00 PM
Found In Egroup: Advanced Software
\ view thread
ID: IN40735 | Access Levels: TechConnect FactoryTalk View SE: FactoryTalk Diagnostic Audit Logging to ODBC
Posted By Philip Hamilton Jun 09, 2026 08:43:00 AM
Found In Egroup: Advanced Software
\ view thread
Most people have the concept of a Local/Remote or Operator vs Automatic control as illustrated below with a two-position maintained selector switch. It would require operator intervention to change the "mode" from Operator to Automatic and back to Operator again. Command Source, PCMDSRC, is built-in ...
Posted By Philip Hamilton Jun 05, 2026 10:02:00 AM
Found In Egroup: Legacy
\ view thread
I just imported the PV550 into a new project. Maybe try doing it on a different PC?
Posted By Philip Hamilton Jun 05, 2026 09:54:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Rockwell (ElectroCraft) S663-1A+2000LD+FRS28-10:1 DAGE,model 005,43-0669
Posted By Philip Hamilton Jun 03, 2026 08:25:00 AM
Found In Egroup: Legacy
\ view thread
send it