List of Contributions

Shaun

Contact Details

Shaun


My Content

1 to 2 of 2 total
Posted By Shaun Sep 25, 2025 09:36:00 AM
Found In Egroup: Installation & Activation
\ view thread
Filip, I will have a look at the technote... They do not connect even though both can ping each other via IP Add and device name, firewalls are disabled on both machines connected via a switch to each other only. ATB Shaun..... -------------------------------------------
Posted By Shaun Sep 24, 2025 05:52:00 AM
Found In Egroup: Installation & Activation
\ view thread
I currently have an XP machine with Panel Builder 32 V03.83.00 (Build 7) installed. We need this to be able to carry out some work for a customer. They also require modifications to the PLC so we have tried using the RSLogix 500 but this comes up with "Fatal Error! The copy protection licence for the ...