Posted By
Shaun
Sep 25, 2025 09:36:21 AM
Found In
Egroup:
Installation & Activation
\
view thread
Filip, I will have a look at the technote... They do not connect even though both can ping each other via IP Add and device name, firewalls are disabled on both machines connected via a switch to each other only. ATB Shaun..... -------------------------------------------
|