List of Contributions

Awadi

Contact Details

Awadi


My Content

1 to 3 of 3 total
Posted By Awadi Jun 25, 2025 01:25:00 AM
Found In Egroup: Automation Control
\ view thread
HI Nmeistrup, I would like to indicate that the control panel installed indoor with an AC. The room ambient temperature is 25 C, the control panel has a good forced ventilation system. The adjacent other types of point IO modules (like analogue inputs and digital inputs) in ...
Posted By Awadi Jun 17, 2025 02:47:00 AM
Found In Egroup: Automation Control
\ view thread
The temperature of module 1734-OE2C has reached 53°C, whereas adjacent other types of point IO modules in the same panel are operating below 40°C. This means that the elevated temperature is not related to ventilation or ambient panel conditions. Additionally, 3 out of 8 modules of this type have ...
Posted By Awadi Jun 17, 2025 02:46:47 AM
Found In Library: Automation Control