Posted By
Awadi
Jun 17, 2025 02:47:00 AM
Found In
Egroup:
Automation Control
\
view thread
The temperature of module 1734-OE2C has reached 53°C, whereas adjacent other types of point IO modules in the same panel are operating below 40°C. This means that the elevated temperature is not related to ventilation or ambient panel conditions. Additionally, 3 out of 8 modules of this type have ...
|