List of Contributions

Eduard Polyakov

Contact Details

Eduard Polyakov


My Content

1 to 20 of 24 total
Posted By Eduard Polyakov Feb 18, 2026 08:30:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Scott! I think this can be achieved if you already have a separate Layer 3 switch to do inter-VLAN routing. Then you can configure routing rules in FTRA to direct the Stratix 4300 to that switch as a next-hop router to reach other VLANs. For example, the LAN interface is assigned an IP address ...
Posted By Eduard Polyakov Jan 21, 2026 07:59:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Scott, One of the digital outputs is activated when the router is online and connected to the FTRA infrastructure. The output is ON if the access is allowed (regardless of the VPN session active or not). I wasn't able to find any email notification options in FTRA but maybe you ...
Posted By Eduard Polyakov Aug 27, 2025 10:14:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
I think so, my guess is that it gets assigned by the Hub dynamically. Sorry I don't have access to a device to try right now -------------------------------------------
Posted By Eduard Polyakov Aug 27, 2025 09:59:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
If it was registered to the domain, you should see it as Offline device in the Domain Explorer - Devices View -------------------------------------------
Posted By Eduard Polyakov Aug 27, 2025 07:23:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Scott, What is the firmware version? For the latest firmware 6.x, the registration ID / password should be displayed (if not registered yet) when you go to the 4300 webpage (local access), FT Remote Access page and click Connect. For fw 4.x you have to use the local method to ...
Posted By Eduard Polyakov May 29, 2025 07:28:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Marty, You can use the Wi-Fi option without a SIM card. The manual should be edited to make it more clear.
Posted By Eduard Polyakov May 18, 2025 01:51:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Jacob, 1783-NATR supports ICMP (pings), HTTP, HTTPS and EtherNet/IP (TCP UDP 44818, TCP/UDP 2222) without custom rules. For other protocols, the limit is 5 custom rules per translation and you cannot have more. https://support.rockwellautomation.com/app/answers/answer_view/a_id/731351/ ...
Posted By Eduard Polyakov May 18, 2025 01:43:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Hello, Please see if any of these options work in your environment: Option 1: configure a static route on your Wi-Fi router, not on the 5200. You need a route to 192.168.10.0/24 with the next hop 192.168.1.250. Your router may allow to add static routes. The switch should keep the default gateway ...
Posted By Eduard Polyakov Feb 20, 2025 09:58:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Amol, Some parameter values are described in the EDS file, for example EnumXXXX sections. The files are in this location: C:\Users\Public\Documents\Rockwell\EDS, you can see which one by looking at the switch properties in Linx. But no description for the Power Supply. (My guess is that there ...
Posted By Eduard Polyakov Jan 22, 2025 08:44:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Is the mask on EN2TPs set to 255.255.255.0? If yes, try to use the same mask on the PC when connecting locally
Posted By Eduard Polyakov Jun 26, 2024 08:34:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Kelvyn, Looks like there is a difference how the interfaces are ordered in BRIDGE-MIB and ifName objects in the IF-MIB. I believe this is unique to the Stratix 5700 platform with two Gig ports. The best solution is for the management software to refer to the actual interface names instead ...
Posted By Eduard Polyakov May 07, 2024 09:57:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Kelvyn, Do you know what SNMP OID is being used that return the incorrect information? I did some quick tests with snmpwalk, and at least for some OID it enumerates all interfaces correctly. This is for 5700 1783-BMS20CGN IOS 15.2(8)E2. For example: .1.3.6.1.2.1.31.1.1.1.1.1 = String: ...
Posted By Eduard Polyakov Mar 21, 2024 08:16:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Dimitri! This looks like an anomaly but I would still verify configuration on switches: If all VLANs are actually created on the switch 224 (with the "show VLAN" command) Double check trunk port settings across all switches in the ring (native, allowed VLANs) Compare "show interface ...
Posted By Eduard Polyakov Nov 30, 2023 06:46:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
ILPOWER is related to the PoE (Inline Power). This KB says the reason is improper grounding. https://rockwellautomation.custhelp.com/app/answers/answer_view/a_id/1138928/loc/en_US#__highlight Cause Stratix switch does not have proper grounding or is not grounded at all Solution Ground ...
Posted By Eduard Polyakov May 26, 2023 07:18:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Michael, The PRP design guide and the application technique are a good start. The guide has some examples of star/linear/ring topologies with PRP, and what is not allowed with PRP. IAB helps when designing a large system with PRP. I would recommend going thru its labs first to get familiar with ...
Posted By Eduard Polyakov Mar 20, 2023 08:02:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
You can redirect any CLI output to a file using TFTP, FTP, SCP and other protocols, or write to a file in the internal flash or SD flash. If running a TFTP server on the PC: show logging | redirect tftp:// / The file will be in the TFTP root folder. Need to allow TFTP thru the firewall. ...
Posted By Eduard Polyakov Feb 18, 2023 07:53:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Jan, For CIP (EtherNet/IP), you can start with this document Ethernet Reference Manual (ENET-RM002) The main part of this document provides a good overview of Ethernet, TCP/UDP, IP, network infrastructure and so on. Appendix A gives an overview of CIP application layer RA ...
Posted By Eduard Polyakov Aug 12, 2022 07:40:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Steven, I would also look at the Stratix user manual chapter 3 - NAT - Configuration Overview. It has diagrams for each use case, including same or different VLANs. Stratix Managed Switches User Manual (1783-UM007)
Posted By Eduard Polyakov Jul 06, 2022 07:03:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Stratix 5800 Advanced catalog numbers also have RedBox feature in the latest firmware: 1783-MMS10A, 1783-MMS10AR, 1783-MMS10EA, 1783-MMS10EAR
Posted By Eduard Polyakov May 27, 2022 08:00:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Duncan! Are Stratix switches licensed in FTNM? Also, if you have REP topology in FTNM, it should monitor and show REP faults even without SNMP traps (will check every periodic scan, not immediate alarm like with traps). Have to license REP switches for any REP alarm to work. If you do have REP switches ...