List of Contributions

Kelvin

Contact Details

Kelvin


My Content

1 to 20 of 50+ total
Posted By Kelvin May 24, 2022 11:48:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi, I understood that Rockwell knowledge ID: QA48169 discussed this function already. which is to issue the ( ExecuteCommand "command string" ) command from a HMI client display (either with /ZA or not) However, what is the solution if an event needs to trigger an external application ( such as Notepad.exe) ...
Posted By Kelvin May 19, 2022 07:26:00 PM
Found In Egroup: Advanced Software
\ view thread
Thanks, Doug, It works. Step 1: from Display Clients --> WorkStation --> Create a new Workstation Client ( Say Studio 5000 as my example below) Step 2: from Terminal --> Select "Studio" Workstation Client --> Enter the Workstation IP Address you have to make sure the Workstation RDP is allowed ...
Posted By Kelvin May 19, 2022 06:14:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi, I have followed the Thin Manager training manual. it seems all applications need to be installed on the RDS Server or have URL connections (like FT View Client, VantagePoint, etc). for a simple example, if the RA Studio 5000 was installed in EWS only ( instead of on the RDS Server), is it possible ...
Posted By Kelvin Mar 29, 2022 01:08:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Kristopher, It is better to follow the Rockwell recommended architecture (enet-td001), which has been tested with Rockwell, CISCO and Panduit. normally, servers (DC, DHCP, DNS, HMI, VP, EWS) should be installed in the IDC on the OT side (Industrial zone). but the MES could be on the IT side. ...
Posted By Kelvin Mar 04, 2022 01:21:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, you can increase from 17 to higher. Can't you? ------------------------------ Kelvin ------------------------------
Posted By Kelvin Feb 22, 2022 03:36:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Thanks, Lesley, the most valuable answer I got. BTW, if the network switches are in the DLR ring (not DLR trunking). will the CIP VLAN and Management VLAN need to combine as one single VLAN? I think it is the only way as the DLR ring only supports a single VLAN. ------------------------------ ...
Posted By Kelvin Feb 21, 2022 03:15:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Thanks, AN. I noted your comments, but Stratix 5700 has no issue with 1G speed. and certainly, 5400 is the best, but 5700 is supported as well. it must be some other differences to choose between REP and DLR Trunking. in my experience, REP is for the switch levels and DLR is the device level. however, ...
Posted By Kelvin Feb 20, 2022 11:05:10 PM
Found In Library: Networks
Posted By Kelvin Feb 20, 2022 11:05:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Hi, Network expert, It might be a dumb question to you, from page 42 of ENET-AT007D-EN-P.pdf. DLR can be configured as VLAN Trunking and the performance is better than REP ring. why choose REP? The DLR VLAN Trunking is good enough for most of industrial automation. If I have 1 PLC processor and ...
Posted By Kelvin Feb 14, 2022 02:47:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
the 1st screenshot is from the 1783-ETAP1F user manual 1783-td001_-en-p 2nd one is from google. ------------------------------ Kelvin ------------------------------
Posted By Kelvin Feb 14, 2022 02:46:48 PM
Found In Library: Networks
Posted By Kelvin Feb 12, 2022 04:14:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Rafel, see screenshot below. I think it does not matter as long as the cable is Multi-mode. 1783-ETAP1F/2F supports both 62.5 and 50. ------------------------------ Kelvin ------------------------------
Posted By Kelvin Feb 11, 2022 04:09:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Recently, I have a discussion with other automation engineers and network engineers. they said that only one VLAN is allowed for each single REP segment. that surprises me. After read through RA textbook [enet-td005_-en-p (REP Design Guide)]. it seems true. Figures 3 to 6 on pages 6 & 7 all indicate ...
Posted By Kelvin Feb 10, 2022 03:35:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Thanks, I do read through the user manual. it has some kind of ambiguity whether the node counts are for each network port or the whole processor. I did a test and confirm the Node count is for the whole processor. see screenshot below. not sure whether the IAB PlantPax wizard will capture this warning ...
Posted By Kelvin Feb 09, 2022 08:33:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Hi everyone, I do understand there are a few RA technotes discussed this topic and the 1756-um543 user manual describes how to count the nodes. but I am still confused about the actual node number. take 1756-L84ES as an example, the Ethernet/IP nodes supported is 250. Does this 250 refer to the ...
Posted By Kelvin Feb 09, 2022 08:32:51 PM
Found In Library: Networks
Posted By Kelvin Oct 27, 2021 12:04:00 AM
Found In Egroup: Automation Control
\ view thread
let's say our customer has 20 identical production lines. it seems I uploaded the PLC program for Line 1, and download to Line 2 and save it. I am not able to go back to Line 1 online immediately. the only way back to Line 1 is via re-download the same program to Line 1. in this case, I have to maintain ...
Posted By Kelvin Oct 19, 2021 04:40:00 AM
Found In Egroup: Automation Control
\ view thread
Having been using FT View SE for many years, I realized that View ME has no such important security feature. when Panelview Plus starts, the "DEFAULT" user is logged in, there is no way you can change to other users, such as OPERATOR automatically. in SE, we can use a command " login OPERATOR Password ...
Posted By Kelvin Apr 01, 2021 07:43:00 AM
Found In Library: Advanced Software
Posted By Kelvin Mar 25, 2017 07:11:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Summary: Switch-for-Automation or Virtual-Desktop-for-Automation Hi Network Guru, I have one control system already commissioned, but the network has problem once few weeks. I studied the network related documents and a bit of confusion of which smartport to select. One ...