Hello, Parameter number 2[BOOTP] of the 22-COMM-E Ethernet adapter should be set to 1 = Enabled to allow DHPC/BOOT software to detect the hardware, whose IP address needs to be configured. To access parameters in the 22-COMM-E adapter, an external HIM, or CCW software + 1203-USB serial communications ...
|