List of Contributions

J G

Contact Details

J G


My Content

1 to 20 of 31 total
Posted By J G Mar 11, 2025 09:22:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, The key parameters to set when using a PowerFlex 750 class drive on a winder application are summarized in PowerFlex 750 Series: Speed / Torque Modes The SLAT modes should be used to avoid runaway conditions in case the material breaks. Inertia Compensation, Inertia Adaptation and ...
Posted By J G Aug 09, 2024 05:25:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, Fault 4028 means that the SMC-50 has detected a problem coming from DPI port 4, which corresponds with physical port/slot 9, where the 20-COMM-ER adapter modules reside. From the thread it reads "sometimes"...That could infer a random pattern of annunciation of fault 4028. Fault ...
Posted By J G Jun 24, 2024 09:02:00 AM
Found In Egroup: Automation Control
\ view thread
Hello there, The EK-44395 Hall-effect speed sensor outputs a TTL signal and is the only one from the Rockwell Automation portfolio specifically mentioned in the Rockwell documentation to be suitable for use as a direct input to the DynamixTM 1444-DYN04-01RA module. Hall-Effect Sensor EK-44395 ...
Posted By J G Apr 22, 2024 05:12:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
It may be possible to adjust parameter 37[Load Type (SMB)] when some problems are encountered during braking, depending of the application. Equally, parameter 38[High Eff Brake (SMB)] maybe useful when braking is applied to high-efficiency motors and relates to the counter EMF produced by these ...
Posted By J G Mar 20, 2024 11:58:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
What are the references or catalogue numbers of the filters used? What is the approximate motor cable length? Are those filters installed upstream or downstream the drives? ------------------------------ J G ------------------------------
Posted By J G Dec 11, 2023 10:45:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, please note that for a 700-K control relay, all internal NO and NC contacts, and also all the internal NO and NC contacts with front mounted NO and NC contacts meet the IEC 60947-5-1 criteria for Mechanically linked performance. More information on this via Mechanically linked contacts ...
Posted By J G Jul 27, 2023 04:53:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, as pointed out on your initial post, the implementation of that application requirement would be possible configuring the MOP (Motor Operated Potentiometer) feature of the PowerFlex 755 with the help of 2 digital inputs. In the scenario presented, it looks like there are not spare inputs ...
Posted By J G Jul 14, 2023 10:43:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, Can you please confirm the full catalogue numbers of the MPL servomotor and the feedback cables? That information will help to fully understand the system you are working with and how to best assess potential alternatives... ------------------------------ Jose Garcia Remote Support ...
Posted By J G Jul 14, 2023 09:02:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Choong, I cannot find any indication of the start up sequence being inconsistent within different power rated Kinetix 5500 servo drives. By product design, the start up sequence shall apply equally in principle to all the power ratings. It is still highly recommended to apply first the Control ...
Posted By J G Jul 13, 2023 08:55:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, please note that the local Rockwell distributor or commercial channel should be the first point of contact to discuss the exact replacement of a PowerFlex 700S phase II drive with a more modern drive. Please also note that the parameter set, terminal connections, physical dimensions ...
Posted By J G Jul 11, 2023 09:02:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, the power up sequence of the Kinetix 5500 servo drive, as mentioned early on this thread, is clearly documented on Publication Kinetix 5500 Servo Drives User Manual. By design specifications, the Kinetix 5500 servo drive needs to be powered up following that order. After applying the ...
Posted By J G Jun 26, 2023 05:15:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Feedback appreciated Zissis. Glad to know it worked out eventually. ------------------------------ Jose Garcia Remote Support ------------------------------
Posted By J G Jun 21, 2023 03:27:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
EDIT: linkified for convenience -FL I think one thing missing here is to link the value of Analog Input 1 (parameter 800) to parameter 10 [Speed Ref 1]. This action is confirmed on Technical note https://rockwellautomation.custhelp.com/app/answers/answer_view/a_id/441489 On this specific ...
Posted By J G Apr 05, 2023 04:28:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
The PowerFlex 525 drive comes with a digital input built into the terminal block (terminal 7) able to read pulse train signals up to 100 kHz at 24V. PWM (Pulse Width Modulation) is a general term that refers to the way that most of the AC typical variable speed drives operate at the inverter section ...
Posted By J G Mar 03, 2023 04:37:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thanks Nelson for your comments. Apologies, one of the documents referenced is internal and company policy does not allow to share this content within this public communication channel. I understand your concerns as well. I would like to suggest that maybe the next action to make progress ...
Posted By J G Feb 24, 2023 10:11:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
EDIT: removed external formatting -FL Hello, there is some conceptual guidance on how to apply a Speed Trim Follower scheme with AC drives via the following document: https://literature.rockwellautomation.com/idc/groups/literature/documents/wp/drives-wp001_-en-p.pdf This other technote includes ...
Posted By J G Feb 14, 2023 09:07:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
For externally mounted braking resistors, the recommendation is to protect the drive from resistor temperature rise. This is done typically by a normally closed contact from an internal thermostat in the resistor. This signal is often used to open a contactor upstream the drive and remove the supply. ...
Posted By J G Feb 02, 2023 10:17:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
EDIT: updated broken link to the first mentioned technote -FL Hello, There are many options to be addressed when handling high inertia loads. Many generic considerations are mentioned on PowerFlex 7 series, PowerFlex 40 1336S & 1336F: Guide line :to handle a high-inertia load Dynamic braking ...
Posted By J G Dec 21, 2022 05:29:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, Thanks for sharing this problem. It looks as if the drive is being used within a Pump Jack oil well application. I am hoping this thread could be visible by other Engineers that have used the PowerFlex 755 drive on this particular type of application, very common I believe in countries ...
Posted By J G Nov 15, 2022 07:28:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, one of the most common load sharing techniques is the speed leader/torque follower described previously. That principle is also applicable to the PowerFlex DC drives. There is further detailed information available from Load Sharing between PowerFlex DC Drives where key parameter settings ...