List of Contributions

Michael Miller

Contact Details

Michael Miller


My Content

1 to 20 of 26 total
Posted By Michael Miller Jul 15, 2025 09:37:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Hermse, Make sure all of your cards have the setting disabled for 'Major fault on controller if connection fails while in Run mode.' Otherwise, if you think there's something wrong with your project, you could export the entire project from Studio 5000 as a .L5K file and import to recreate the ...
Posted By Michael Miller Jul 15, 2025 09:30:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, I'm looking for an adapter to convert a CompactLogix rack into remote I/O for an existing ControlLogix processor. Does such a thing exist? FTAs weren't used with the CompactLogix I/O, so I'm trying to avoid rewiring all of the I/O to new cards... Thanks!
Posted By Michael Miller Jul 11, 2025 09:30:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Julia, Is there an application you use to monitor the Directory's sync status or do you use the FT diagnostic logs? Thanks!
Posted By Michael Miller Jul 10, 2025 02:16:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi Julia, Really appreciate the suggestions. For your item 1, are the effective permissions configured in the communication settings for each data server? I'm not sure where that is located. And for item 2, I didn't see any logoff macros configured for any user groups in the Runtime Security. Did ...
Posted By Michael Miller Jul 10, 2025 08:29:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, On my FactoryTalk SE version 10 distributed application with PlantPAx version 3.5.1 objects, a user who has FT engineering credentials suddenly loses the ability to perform certain actions such as faceplate mode changes or acknowledge alarms. Odd enough, the same user is still able to change ...
Posted By Michael Miller Feb 16, 2024 08:56:00 AM
Found In Egroup: Networks
\ view thread
Hi everyone, On two occasions now we have had wide-spread loss of visibility events on our FactoryTalk v10 SE HMIs. Both times we found thousands of FT diagnostic logs reporting "connection could not be established on route ControlLogix..." The issue resolves itself within a minute or so. The ...
Posted By Michael Miller Nov 02, 2023 07:44:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, How would I setup a SQL query to retrieve disabled alarms with disabled time, disabled user and comments for FactoryTalk View SE v10? The alarm status explorer has this info but you have to click on each alarm to get the disabled time/user. Not very useful for reports. Thanks! ----- ...
Posted By Michael Miller May 22, 2023 08:17:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, Does Rockwell recommend using whitelisting software with a FactoryTalk version 10 environment? If so, any suggestions or things to avoid? Thanks. ------------------------------ Michael Miller ------------------------------
Posted By Michael Miller Feb 14, 2023 09:58:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, Is it possible to remotely reset the system health of a T9110 AADvance processor? I'm using Workbench 1.0 with firmware 1.34. Thanks, ------------------------------ Michael Miller ------------------------------
Posted By Michael Miller Jan 31, 2023 07:18:00 AM
Found In Egroup: Automation Control
\ view thread
I have a redundant 1756-L75 ControlLogix setup, where my CPU load around 75%. In order to reduce the load I'm considering disabling the 'Synchronize redundancy data after execution' setting in each program. My understanding is this shouldn't be an issue since my periodic tasks are between 250 & 1500ms ...
Posted By Michael Miller Dec 12, 2022 02:22:00 PM
Found In Egroup: Automation Control
\ view thread
Hi Phillip, Is there a way to determine what the module fault code was for past events? It does recover on it's own, which sounds like is leaning more towards a comm fault. There are a couple dozen event logs in the remote rack's EN2T indicating connection time out, error receiving data, attempting ...
Posted By Michael Miller Nov 30, 2022 07:17:00 AM
Found In Egroup: Automation Control
\ view thread
Thanks. Sounds like the only way to see CPU % is using the faceplate. Very odd. Hopefully that's corrected in v35 for customers not using FT View. ------------------------------ Michael Miller ------------------------------
Posted By Michael Miller Nov 29, 2022 07:58:00 AM
Found In Egroup: Automation Control
\ view thread
Thanks, Phillip. Does that still work if I'm not using FactoryTalk View SE? I could probably setup a PanelView with ME if that would work. Or is the % CPU parameter visible in the AOI? ------------------------------ Michael Miller ------------------------------
Posted By Michael Miller Nov 28, 2022 10:33:00 AM
Found In Egroup: Automation Control
\ view thread
Hi everyone, I'm wondering how I can see the CPU utilization on a pair of v33.012 redundant 1756-L85Es? When the processor was in simplex at v31, CPU was around 5%; however, judging by the task scan time I'd say it's around 50% now (taking 240ms for a 500ms periodic task, 10x the time in simplex). ...
Posted By Michael Miller Nov 21, 2022 07:37:00 AM
Found In Egroup: Automation Control
\ view thread
Bill, Might have found a relevant Microsoft thread that provides a solution. Right-click your desktop, go to Display Settings and adjust the % scale under the Scale and layout section. You can also apply a custom scale by clicking on Advanced scaling settings. https://answers.microsoft.com/en-us ...
Posted By Michael Miller Nov 17, 2022 08:25:00 AM
Found In Egroup: Automation Control
\ view thread
Hi everyone, I have a redundant 1756-L71 (v24.52) system with a single remote rack. Diagram attached. The problem I'm seeing is about once every month or so we see multiple cards in the remote rack faulting. Some times it's as frequent as every other day, other times there's 2+ months between events. ...
Posted By Michael Miller Nov 15, 2022 11:18:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Bill, Are you by chance opening the software locally then accessing it via remote desktop? I've noticed when I open Studio on my laptop, then RDP into it from my main PC I'll see what you're describing until I restart the software. That seems to be something Microsoft hasn't perfected with monitor ...
Posted By Michael Miller Nov 14, 2022 12:36:00 PM
Found In Egroup: Automation Control
\ view thread
Thanks, Phillip. I did open a ticket and they also recommended a firmware upgrade to v11.003 (latest). By the way, existing firmware was 10.7.217021900, hardware rev 3.1. ------------------------------ Michael Miller ------------------------------
Posted By Michael Miller Nov 10, 2022 12:58:00 PM
Found In Egroup: Automation Control
\ view thread
Good afternoon, Today I found a faulted 1756-EN2TR/C (v3.001) that displayed the message "Cycle Power to Unit Assert in File DummyFaultListener.cpp line 172." I was able to power cycle the entire chassis and replace the 1756-EN2TR to resolve the issue. Does anyone know what the message on the faulted ...