Were they able to try a spare motor? If the trouble goes away with a different motor, I would suggest that the motor bearings were starting to fail. Did the motor have a brake on it? Even if they were not using the brake, the wear on the disc spinning in the housing can cause enough drag that might ...
|