List of Contributions

dsowell

Contact Details

dsowell


My Content

1 to 4 of 4 total
Posted By dsowell Oct 01, 2021 04:16:00 AM
Found In Egroup: Networks
\ view thread
Hi Rob, I have only been cycling the power on the drive with the 22-COMM-D card on it when making changes. The drives attached to it will show F081 faults until the drive I am working with powers back up and they are reset. We have issues with cycling the power on cabinets with multiple Powerflex ...
Posted By dsowell Sep 29, 2021 04:30:00 AM
Found In Egroup: Networks
\ view thread
Hi Rob, Thanks for replying to my question. To answer your questions, the 22-COMM-D is mounted on a Powerflex 40 which in turn has four other drives connected to the Powerflex 40. I am using RSNetworx for Devicenet to program everything. I'm using RSLinx with the 1747-SDNPT set up through Ethernet. ...
Posted By dsowell Sep 22, 2021 12:34:00 AM
Found In Egroup: Networks
\ view thread
I am having an issue with a 22-COMM-D adapter card that I need help on. We had to replace a 22-COMM-D card on a Powerflex 40 drive. This card acts as a communications link to four other drives (set for 5X). Using RSNetworx for Devicenet, the card shows up in the graph O.K. I have tried to download ...
Posted By dsowell Jun 21, 2011 11:34:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Were they able to try a spare motor? If the trouble goes away with a different motor, I would suggest that the motor bearings were starting to fail. Did the motor have a brake on it? Even if they were not using the brake, the wear on the disc spinning in the housing can cause enough drag that might ...