List of Contributions

VerEllen

Contact Details

VerEllen


My Content

1 to 9 of 9 total
Posted By VerEllen Jul 25, 2023 05:18:07 AM
Found In Egroup: Automation Control
\ view thread
Did you enter the verification code after editing the logic? ------------------------------ VerEllen ------------------------------
Posted By VerEllen May 16, 2023 12:37:53 PM
Found In Egroup: Automation Control
\ view thread
That did the trick, Thank you Daniel ------------------------------ VerEllen ------------------------------

CCW

Posted By VerEllen May 15, 2023 01:26:00 PM
Found In Egroup: Automation Control
\ view thread
I get the following message when trying to generate a report. I've tried several different files but this keep popping up. ------------------------------ VerEllen ------------------------------
Posted By VerEllen May 15, 2023 09:33:21 AM
Found In Egroup: Legacy
\ view thread
This is the configuration of the input card. It lists it as Series "A", the physical card says Series "B". Could that be the causing factor? ------------------------------ VerEllen ------------------------------
Posted By VerEllen May 15, 2023 07:03:48 AM
Found In Egroup: Legacy
\ view thread
Here is a look at the schematic ------------------------------ VerEllen ------------------------------
Posted By VerEllen May 12, 2023 06:18:22 AM
Found In Egroup: Legacy
\ view thread
Ryan, Here is a picture of the instruction. ------------------------------ VerEllen ------------------------------
Posted By VerEllen May 12, 2023 05:09:30 AM
Found In Egroup: Legacy
\ view thread
Yes fuzzy logic, They are connected correctly as to the polarity, and nothing is connected to the COM terminals. We will not have another heated container to test until the middle of next week. I will take Ryan's suggestion and move the zones between the PLC and the 1762 and see if I can read the input ...
Posted By VerEllen May 11, 2023 10:24:00 AM
Found In Egroup: Legacy
\ view thread
Ryan, Yes, they are set to voltage. ------------------------------ VerEllen ------------------------------
Posted By VerEllen May 11, 2023 09:09:00 AM
Found In Egroup: Legacy
\ view thread
EDIT: moved to Legacy community -FL I have MicroLogix 1400 with a 1762-IF4 at slot 1. I am trying to monitor current on an HMI. My first two zones (L1 & L2) are connected to the analog inputs on the PLC and my last two zones are connected to the 1762. When running the first two zones (Zones 1 & 2, ...