Posted By
VerEllen
May 12, 2023 05:09:30 AM
Found In
Egroup:
Legacy
\
view thread
Yes fuzzy logic, They are connected correctly as to the polarity, and nothing is connected to the COM terminals. We will not have another heated container to test until the middle of next week. I will take Ryan's suggestion and move the zones between the PLC and the 1762 and see if I can read the input ...
|