List of Contributions

rta53

Contact Details

rta53


My Content

1 to 20 of 44 total
Posted By rta53 May 17, 2023 09:12:00 AM
Found In Egroup: Installation & Activation
\ view thread
Govind, No, rehosting did not work for me. I got a message that the serial number had already been rehosted. Something evidently didn't work properly because it is still in the list of activations. ------------------------------ rta53 ------------------------------
Posted By rta53 May 17, 2023 06:25:00 AM
Found In Egroup: Installation & Activation
\ view thread
Philip, I have asked this before in a separate thread but never got a good answer. How do you delete expired activations? In the past all we had to do was go the the activations folder and delete the lic file and all was good. Now there is no file to delete, at least I can't find one, since Rockwell ...
Posted By rta53 Jun 01, 2022 06:10:00 AM
Found In Egroup: Installation & Activation
\ view thread
EDIT: linkified for convenience -FL Check out Knowledge Base article BF12727. One of our customers had the same issue. I believe we ended up deleting the .rnl files as shown in article BF12152. ------------------------------ rta53 ------------------------------
Posted By rta53 May 31, 2022 05:55:00 AM
Found In Egroup: Installation & Activation
\ view thread
I agree! It used to be a very simple task to remove expired activations. Hopefully this can be addressed. ------------------------------ rta53 ------------------------------
Posted By rta53 May 25, 2022 09:31:29 AM
Found In Library: Installation & Activation
Posted By rta53 May 25, 2022 09:31:00 AM
Found In Egroup: Installation & Activation
\ view thread
Does anyone know how to remove expired activations that use the CodeMeter service? With the old style licensing you simply went to the activations folder and deleted the expired LIC file. See attached screen shot. ------------------------------ rta53 ------------------------------
Posted By rta53 Dec 01, 2011 01:20:00 PM
Found In Egroup: Automation Control
\ view thread
So are you asking me if this is possible or are you suggesting a solution? There are no system tags that show active alarms, acknowledged alarms, etc, that I have found. ##HL41
Posted By rta53 Nov 28, 2011 06:01:00 AM
Found In Egroup: Advanced Software
\ view thread
When you run FTView SE installer there is a step by step guide that shows you how to upgrade. Basically you have to remove your current version of FTV and some other stuff but it's pretty easy to do. As far as needing to upgrade FTV because of upgrading to CLX v19 you shouldn't have to unless you just ...
Posted By rta53 Nov 23, 2011 07:57:00 AM
Found In Egroup: Automation Control
\ view thread
Instead of starting my own thread I thought I would just comment on this one since the original question is what I was planning to ask anyway. For the life of me I don't understand why Rockwell feels the need to complicate something so simple. Ok I get it that there is not an alarm banner in FTView SE ...
Posted By rta53 Jun 27, 2011 09:08:00 AM
Found In Egroup: Automation Control
\ view thread
Summary: Need active alarm indication I have installed some greyscale PanelView Component C600s. I am using the alarm banner and the alarm list. One of the complaints I am getting from operators is that they do not know if an alarm is still active. On the alarm list I show these columns: Alarm Message, ...
Posted By rta53 Apr 06, 2011 08:23:00 AM
Found In Egroup: Automation Control
\ view thread
Fuzzy you beat me to the draw. That's exactly what I was trying to say. Emanuele, you keep mentioning selecting one of the tags. You don't need to do this if you are wanting to change all the tags on a screen. Just do search and replace and it will perform the task on all the tags in the list that meet ...
Posted By rta53 Apr 06, 2011 08:05:00 AM
Found In Egroup: Automation Control
\ view thread
I've done this many times. Do select all and then tag substitution and then search for and replace. I've done this when I copied an existing screen into a new project and needed to change the short cut. In other words if your old short cut was "bob" and you wanted to change all the tags to have a short ...
Posted By rta53 Sep 13, 2010 07:18:00 AM
Found In Egroup: Legacy
\ view thread
Yes I did have the module powered. The problem with stuff like this is that when you don't do it every day you forget a lot, at least I do. The last couple of Flex I/O projects we have done were with Ethernet and Control Logix which are somewhat different. Over the weekend I finally realized one thing ...
Posted By rta53 Sep 10, 2010 11:32:00 AM
Found In Egroup: Legacy
\ view thread
We have a SLC 5/05 based system with a 1747-SN scanner and 2 remote racks with Flex I/O and 1794-ASB adapters. It has been running fine for many years. I am having to add a 1794-IE8 module in rack 1. It is the 8th module in the rack so I have it as Rack 1 Group 7 in my BTR/BTW instructions. I added the ...
Posted By rta53 Aug 31, 2010 12:56:00 PM
Found In Egroup: Advanced Software
\ view thread
Thanks for the info. What I was referring to was that for some reason FT Activation Tool did not get installed when I installed FTView. I went back and looked in the install guide and saw that I could install it manually, which I did. Thanks again for your help. ##HL101
Posted By rta53 Aug 30, 2010 11:40:00 AM
Found In Egroup: Advanced Software
\ view thread
ok that makes sense. Another question. I wanted to make sure that my activation for SE Station was installed however I do not have FT Activation installed on the client computer. Why would that not have installed when I installed FT services? Seems I remember the box being checked at the end of the installation ...
Posted By rta53 Aug 30, 2010 08:53:00 AM
Found In Egroup: Advanced Software
\ view thread
I am in the process of setting up a FTView SE standalone(local) client on a new computer. The installation guide says to backup the application on the development computer and then restore it on the production computer using the application manager. However the application manager is not installed on ...
Posted By rta53 Mar 19, 2010 08:12:00 AM
Found In Egroup: Legacy
\ view thread
Tech 411 wrote: pick a question please... can't address : AB doc creation policy AND scaling AND accuracy AND is it input or output or both AND manual content as for basic and necessary there's always the SCP or SCL instruction. Shrug It's just a lot of acreage to cover in a single ...
Posted By rta53 Nov 30, 2009 09:03:00 AM
Found In Egroup: Legacy
\ view thread
One of the things that has puzzled me for years is why you cannot find any info in regards to scaling the Micrologix analog modules (1762) in any of the manuals. There is a technote about this (Answer ID 19719) but nothing in the manuals that I have found. You would think that something as basic and ...
Posted By rta53 Nov 20, 2009 06:36:00 AM
Found In Egroup: Advanced Software
\ view thread
Thanks. I had seen that technote a couple of days ago and thought it was just referring to the performance monitor in the task manager. I have set up a monitor log for FT. Will see what happens. Hopefully this will help. ##HL101