List of Contributions

Emre Karakaya

Contact Details

Emre Karakaya


My Content

1 to 20 of 50+ total
Posted By Emre Karakaya Jul 10, 2026 06:20:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, How can I change panelloader page with combobox? Is there any example for it?
Posted By Emre Karakaya Jul 03, 2026 03:19:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Xavier, Thanks for the information. We have a similar setup. Our customer wants to retrieve PLC tags from 20 different stations and then use those tags from the tag lists to create 20 different Ethernet/IP stations in the CommDriver section of the Optix HMI. It's actually a simple application. ...
Posted By Emre Karakaya Jul 02, 2026 05:00:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi @LogicIQ, We are distributors. We have examined the product. It has SIM card support. It also appears to have VPN support, but since no project related to this has been done before, I'm writing about it here as well. We need to get approval. Perhaps someone has used such a system before. ...
Posted By Emre Karakaya Jul 02, 2026 03:55:43 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank you for info
Posted By Emre Karakaya Jul 02, 2026 03:01:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hello, We want to collect data from 20 different stations on a single SCADA screen. We need a switch or router that supports SIM cards and connects PLC tags to a common point. I also think we'll need a VPN to retrieve data from the field. Based on all this information, which product can I ...
Posted By Emre Karakaya Jul 02, 2026 02:42:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, The histogram label is displayed vertically. Is it possible to rotate the label horizontally in Optix Studio?
Posted By Emre Karakaya Jul 01, 2026 05:21:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, I would like to communicate with an RFID reader that uses a USB 2.0 connection by writing C# code in FactoryTalk Optix NetLogic. Is it possible to use the USB port available on the Optix device for this communication? If so, could you provide information or an example of how the C# code ...
Posted By Emre Karakaya Jun 23, 2026 12:13:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank you for info @CodeAssist
Posted By Emre Karakaya Jun 22, 2026 08:20:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank you for the information. Besides that, I have another very important question. Currently, FT Optix doesn't have an automatic scaling feature. For example, I can't scale a project I prepared for a 15-inch screen to a 10-inch panel. FT View ME has this feature. In which version will this feature ...
Posted By Emre Karakaya Jun 22, 2026 02:43:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Currently, this is intended to be used on the Optix side, similar to what's in the FT View ME/SE. Is there anyone we can reach who can provide information about which version this will be included in?
Posted By Emre Karakaya Jun 20, 2026 07:41:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, Can we import or export visuals in Optix HMI as .gfx files? This feature exists in FT View Studio. Can we perform the same operation within Optix Studio? If so, is there an example of how to do it?
Posted By Emre Karakaya Jun 05, 2026 05:04:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, We need a printer that can be used with Compactlogix PLCs. We will use this printer to print daily reports on A4 paper. We've seen Zebra brand Ethernet/IP printers, but they are very expensive. Therefore, what are some affordable printer brands and models that we can use with the Studio ...
Posted By Emre Karakaya May 25, 2026 05:10:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi @Xavier Florensa. Thank you so much. Very good application. You’ve made it very simple by using dynamic links this way in the application. Thanks again for your work. -------------------------------------------
Posted By Emre Karakaya Feb 25, 2026 12:23:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Suryawanshi, What should we do if we can't find the working Kepware file? We currently have a PanelView Plus 1000 HMI in the field. Is it possible to access the existing working Kepserver file within Windows CE on this panel and use it on the new PanelView Plus 7 HMI? Thanks. ...
Posted By Emre Karakaya Feb 24, 2026 07:24:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, I converted my PanelView Plus 1000 project to PanelView Plus 7. I uploaded the program to the HMI, but the PLC and HMI are not communicating. When I checked the tags in Kepserver and the project, I noticed that the PLC names appear differently and the tags in the project are not present ...
Posted By Emre Karakaya Feb 23, 2026 03:36:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, I can't change any values ​​in Optixpanel after entering my password. What could be the reason? It worked before. My password is correct. -------------------------------------------
Posted By Emre Karakaya Feb 04, 2026 11:39:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank you for the information. Do you know of any other third-party Historian software that can communicate with Optix? This is a bit urgent, so we need to take action as soon as possible. -------------------------------------------
Posted By Emre Karakaya Feb 04, 2026 05:40:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, Can I keep records of the data I receive from Optixpanel using the Factorytalk Historian SE license? Is there a sample application for this? -------------------------------------------
Posted By Emre Karakaya Feb 04, 2026 02:05:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, I'm going to back up data from the Optix panel to a flash drive. The project includes audit records, alarm history, and recipes. When I back up, will all this data be saved without being lost? -------------------------------------------
Posted By Emre Karakaya Jan 16, 2026 06:23:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, I want to enable the remote access feature of Optix HMI via Factorytalk Hub. I have enabled the "Approve remote access" feature. When I click on VPN, it constantly gets stuck on the "waiting for user authorization" message and cannot get past it. How can I solve this problem?