List of Contributions

Heath

Contact Details

Heath


My Content

1 to 16 of 16 total
Posted By Heath Apr 03, 2026 09:56:00 PM
Found In Egroup: General Discussions
\ view thread
Hey all, Should Engage have more discussion areas? For example ASEM Hardware, Non Asem Hardware, Controllers and IO etc. Was going to post something I discovered today on a 6300P-EW1 Panel PC and sadly there was no appropriate home for this. Thoughts? ------------------------------ Heath ...
Posted By Heath Mar 15, 2026 10:08:11 AM
Found In Egroup: Advanced Software
\ view thread
Blake, absolutely! please and thanks ------------------------------ Heath ------------------------------
Posted By Heath Mar 10, 2026 11:37:00 AM
Found In Egroup: Advanced Software
\ view thread
All, I know there are some posts leading around this subject, but I wanted to ask the community. My question is if using the embedded INfluxDB or embedded MYSQL in an Optix device like an OptixEdge, Embedded Edge Compute or Optix Panel, would external tools like Grafana be able to access the OPTIX ...
Posted By Heath Mar 09, 2026 09:21:35 AM
Found In Egroup: Advanced Software
\ view thread
Great!! looking forward to using some of the PPT content for an upcoming Visualization Roadshow event. -------------------------------------------
Posted By Heath Mar 05, 2026 10:02:53 AM
Found In Egroup: Advanced Software
\ view thread
One thing you can do is leverage the SYSTEM Object. The System object variables can be exposed or displayed in the runtime. By adding it into an Optix project for a 1756 EEC, OptixEdge or Optix Panel you will get access quickly to what's happening while your device is running. ---------- ...
Posted By Heath Feb 06, 2026 05:20:43 PM
Found In Egroup: Advanced Software
\ view thread
@Retzlaff There is the FTRA Widget that can be leveraged that has the Remote Connection Count Variable that will go active if a remote connection is active. This could leverage to have a popup happen to display the warning. You also initiate a text box in the pop up where you could enter in a message ...
Posted By Heath Feb 05, 2026 09:50:41 AM
Found In Egroup: Advanced Software
\ view thread
I have also added the System Property to some of these type projects where resources were a concern like this happens. The System object will expose a lot of details of what's going on inside of a Panel, Optix Edge or Embedded Edge Compute. From there you can datalog or display the resources while the ...
Posted By Heath Jan 23, 2026 06:59:51 PM
Found In Egroup: Advanced Software
\ view thread
A customer of mine had the same issue at times. His issue was resources (RAM) was running low. He streamlined the project a bit and removed nodes and scripts that were not in use. He also did this from the knowledgebase: Alarm Collection Setting The Alarm Collection Enabled property located at ...
Posted By Heath Aug 09, 2025 07:23:20 AM
Found In Egroup: Advanced Software
\ view thread
I had a similar issue the other day where the custom keyboard wouldn't appear via the web presentation engine. It worked initially but after few modifications it did not. I cleared the web browsers cookies and cache and it was back popping up again. -------------------------------------------
Posted By Heath Jul 18, 2025 12:17:00 PM
Found In Egroup: Advanced Software
\ view thread
Example of the FT Remote Access Utility
Posted By Heath Jan 10, 2025 10:08:12 AM
Found In Library: Advanced Software
Posted By Heath Jan 10, 2025 10:08:00 AM
Found In Egroup: Advanced Software
\ view thread
Just wanted to throw this out to the community. Has anyone attempted using Optix with an Automation Direct (Click PLC) or any other controller manufacturer that uses Ethernet IP? Basically would Optix support a controller that has a non RA Ethernet IP interface? Was curious if the OPTIX RA Ethernet IP ...
Posted By Heath Jul 30, 2024 07:48:00 AM
Found In Egroup: Advanced Software
\ view thread
Found this in ASEM's help: Web presentation engine (asem.it) I don't think this is called out yet in the online Optix help files. To display a specific webpage in the browser: Display a specific window using shortcut To directly display a specific window among those available ...
Posted By Heath Apr 28, 2024 06:50:00 AM
Found In Egroup: Advanced Software
\ view thread
Be sure to use the LAN Port on the Optix Panel. The WAN port will not work for PLC connectivity.
Posted By Heath Jan 29, 2024 09:26:00 PM
Found In Egroup: Advanced Software
\ view thread
Well, I completely missed that! Thanks! I see said the blind man EDIT: resized images to be smaller -FL
Posted By Heath Jan 29, 2024 01:29:00 PM
Found In Egroup: Advanced Software
\ view thread
As of of version 1.3 of Optix Studio An Upload Project Feature was added..... Per the release: •As part of the deployment of an application, you can now choose to "Download source project on device" •This allows the project to be uploaded at a later time from any deployed device back to your ...