List of Contributions

Ed Grudzinski

Contact Details

Ed Grudzinski


My Content

1 to 20 of 28 total
Posted By Ed Grudzinski Mar 25, 2026 04:50:41 PM
Found In Egroup: Automation Control
\ view thread
Hi @qinggang, Without knowing the specifics of what virtual network card driver you installed, or what your other network settings might be, it's hard for me to give advice on what to check here. It seems that this driver must be changing some fundamental network setting on your PC, and that change ...
Posted By Ed Grudzinski Mar 16, 2026 07:12:01 AM
Found In Egroup: Automation Control
\ view thread
Hi DAraque, What version of FT Echo do you have installed? The L9 firmware packages require using the latest version which is 4.00.00. You should be able to upgrade to the latest if you have an older version by just installing the latest. All your data should be saved. The newest version contains all ...
Posted By Ed Grudzinski Feb 20, 2026 09:40:30 AM
Found In Egroup: Automation Control
\ view thread
Currently this is the only way to do this via the Logix Designer SDK. -------------------------------------------
Posted By Ed Grudzinski Feb 19, 2026 03:26:22 PM
Found In Egroup: Automation Control
\ view thread
Hi Walke, There is nothing wrong with accessing UDTs, but you cannot specify part of the tag using the path, just the whole tag. In your example the tag would just be "Controller/Tags/Tag[@Name='Pump']" What you do with that depends on what you're trying to accomplish: If you want live data, you ...
Posted By Ed Grudzinski Jan 22, 2026 11:20:40 AM
Found In Egroup: Automation Control
\ view thread
This isn't a restriction so much as it's just how Ethernet/IP works. 127.0.0.1 is the loopback address and always points to your local machine. So this works because Windows knows where to go and just connects to itself. The help for FT Echo does have a section for IP addresses that explains the ...
Posted By Ed Grudzinski Jan 22, 2026 08:21:23 AM
Found In Egroup: Automation Control
\ view thread
OK, if it shows up in FT Linx that's good. Try configuring a single controller in Echo using the default IP address, which is 127.0.0.1 and see if that can download. -------------------------------------------
Posted By Ed Grudzinski Jan 22, 2026 07:05:40 AM
Found In Egroup: Automation Control
\ view thread
When you install Echo it should automatically configure FT Linx and a few other things needed to connect all of these apps together. You should have an "EmulateEthernet" entry in FT Linx created for you. If not, it's possible Echo was installed before FT Linx. The easiest fix right now might be to ...
Posted By Ed Grudzinski Jan 20, 2026 03:39:51 PM
Found In Egroup: Automation Control
\ view thread
Just to verify: Are you able to open Logix Designer on the same machine you are running your C# application on and download to the controller from there? If that doesn't work then we should get it working first prior to using the SDK to download, as the SDK will use Logix Designer under the hood. ...
Posted By Ed Grudzinski Jun 25, 2025 07:34:00 AM
Found In Egroup: Automation Control
\ view thread
As mentioned above please make sure your license is available. You can check by clicking Help->About on the Dashboard. Please make sure whatever PC or VM that is hosting Echo has enough resources. If on a VM try allocating more RAM and CPU cores. You can also try shutting down applications that ...
Posted By Ed Grudzinski Mar 20, 2025 07:15:00 AM
Found In Egroup: Automation Control
\ view thread
When you shut down an Echo controller, it must reach a stopping point and save all of its current state to disk before the shutdown can be successful. If it doesn't have time to do this, then the current state and program are lost, and you'll need to redownload and start over. This process can take some ...
Posted By Ed Grudzinski Apr 23, 2024 07:25:00 AM
Found In Egroup: Automation Control
\ view thread
Chip, I'm glad to hear your positive feedback using FT Echo! I don't have anything to share with respect to the two suggestions you made (Ethernet module, and supporting past FW), but I have passed these on to the product team. Knowing what our customers are interested in helps us to plan future ...
Posted By Ed Grudzinski Apr 17, 2024 06:03:00 PM
Found In Egroup: Automation Control
\ view thread
Chip, thanks for the response. As you discovered, Echo cannot communicate with physical devices either controllers or I/O. This is a limitation of the product as stated in our documentation. I think your only solution using Echo right now is to simulate your whole system using only Echo controllers ...
Posted By Ed Grudzinski Apr 17, 2024 12:26:00 PM
Found In Egroup: Automation Control
\ view thread
Hi Chip, Thank you for your feedback about Echo. I'd like to see if I can help you find a solution. Can you provide any more details about what devices you'd like Echo to be able to communicate with? What specific restrictions are you running into?
Posted By Ed Grudzinski Feb 08, 2024 07:06:00 AM
Found In Egroup: Automation Control
\ view thread
If you are able to upgrade to FT Echo 3.00.00 we made a change that allows you to specify whatever IP address you want using the dashboard. This was always possible using the API in previous versions, so now it has parity in the dashboard. Note that you'll still have to have at least one controller ...
Posted By Ed Grudzinski Jan 30, 2024 07:07:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Carl, Thanks for responding. Unfortunately, at this point, I don't have any information to communicate regarding a breakpoint feature in FT Echo. I will communicate your feedback with the product team.
Posted By Ed Grudzinski Nov 29, 2023 07:42:00 AM
Found In Egroup: Automation Control
\ view thread
Carl, If there are specific problems you are having with FT Echo please open a new thread to describe them and I can try to help you address them. Thank you for your feedback! ------------------------------ Ed Grudzinski ------------------------------
Posted By Ed Grudzinski Nov 08, 2023 03:11:00 PM
Found In Egroup: Automation Control
\ view thread
Hello SKY, To access program tags you want to use a string like "Controller/Programs/Program[@name='programName']/Tags/Tag[@name='tagName']" I spoke with the dev team about this, and they will be adding more documentation around this in a future release. Thanks for the question, and ...
Posted By Ed Grudzinski Oct 31, 2023 01:05:00 PM
Found In Egroup: Automation Control
\ view thread
Are you running as a normal Windows user or as Administrator? Are you running the Echo Dashboard with limited privileges? A couple things to check: Verify that you have FactoryTalk Services Platform installed. It should be part of the FactoryTalk Echo installation media. Looking ...
Posted By Ed Grudzinski Oct 24, 2023 06:53:00 AM
Found In Egroup: Automation Control
\ view thread
Could you give us a few more details? You mentioned installing Echo on a different computer. Do you have multiple PCs involved here? Where are you downloading from/to and what is installed on each? You may already be aware of this, but just a few notes: in order to use the Echo Dashboard to download, ...
Posted By Ed Grudzinski Oct 10, 2023 08:22:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Jhon, You may already be aware of some of this but let me clarify what's going on with the versioning here. The Service API and Controller API versions are independent of each other and also can be independent of the overall Echo product version. The Service API version is tied to the version ...