List of Contributions

⚙ Andrew Wu

Contact Details

⚙ Andrew Wu


My Content

1 to 20 of 50+ total
Posted By ⚙ Andrew Wu Jul 17, 2026 05:25:16 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Parker, I generally solve this by invoking a reset for each child controller from the master - if you really don't want to add a bunch of references to external scripts, consider using a boolean trigger on the child controllers e.g. set "ResetNow" property from False to True, "OnResetNowUpdated" ...
Posted By ⚙ Andrew Wu Jul 03, 2026 10:18:45 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Campbell, We recently released some detailed documentation on how to use the Roboguide CAM IF connection protocol, you can find this here - https://store.sim3d.com/tutorials/fanuc_roboguide_achieving_cosimulation_via_a_cam_if_connection. This was/is a relatively new feature, hence the delayed response. ...
Posted By ⚙ Andrew Wu Apr 16, 2026 05:49:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Tom, Glad to see that you and Friedrich have found the cause of the issue. I agree that a future update is necessary to ensure data is transferred reliably regardless of localization. I have plans to overhaul our robot comms protocol to send raw bytes instead of strings, which I believe would ...
Posted By ⚙ Andrew Wu Apr 14, 2026 10:07:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Tom, Based on the screenshot, it looks like the Type is being specified correctly (double is equivalent to 64-bit float). I have attached another test model for you to try which should print out the exact string value for all tags (joint & IO) before the conversion happens. From this we will ...
Posted By ⚙ Andrew Wu Apr 13, 2026 08:23:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Tom, I inspected your E3D model but couldn't see any immediate problems. Interestingly, if we convert the robot angles displayed in the RobotStudio slider UI to Radians, we get very close to the values coming across in the IO Browser - just with the decimal place missing. Signage seems to be ...
Posted By ⚙ Andrew Wu Apr 13, 2026 05:04:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Tom, This is actually somewhat of a positive sign for us, as it indicates that it wasn't any recent 2026 changes that caused this. 2025 was well used and tested, so it is pointing towards something being off on your side. I noticed in one of our support tickets where your issue was forwarded ...
Posted By ⚙ Andrew Wu Apr 12, 2026 04:37:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi Tom, The Emulate3D team is currently waiting on ABB RobotStudio license renewals, so unfortunately we're unable to test locally at this time. Could you try in 2025 with version 4.0.0 of the Robot Emulation Servers script and version 4.10.8 of the Robot Framework script (higher versions are compatible ...
Posted By ⚙ Andrew Wu Feb 05, 2026 10:42:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Slejska, Are the loads hollow at the center? The robot tool does a Ray Pick from top down, and if the loads are hollow the Ray will end up going past the load and detecting the conveyor below instead etc. You should be able to modify the LookDirection and LookOffset via properties on your ...
Posted By ⚙ Andrew Wu Jan 08, 2026 10:15:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Paul, Glad to hear! The member of our team experiencing the same issue has also confirmed the latest update has fixed things. I will be able to release a non-beta version of 4.10.7 once it has been approved by QA, probably sometime next week. -------------------------------------------
Posted By ⚙ Andrew Wu Jan 08, 2026 10:09:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Will, Do you have a (virtual) Robot Controller in your MotoSim workcell? In order to generate the Joint Angle tags for a workcell, the plugin requires a controller to be present, not just the Robot model itself. -------------------------------------------
Posted By ⚙ Andrew Wu Jan 07, 2026 09:23:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Paul, This issues seems to have happened to a handful of users since version 4.10.6 of the Robot Framework was released, but not frequently enough for us to be able to identify the cause. I have released a speculative fix just now in version 4.10.7-beta.1. Please could you update to this version ...
Posted By ⚙ Andrew Wu Sep 30, 2025 06:21:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Suryan, It comes down to a few things: TileType needs to be Transfer in order for the Pod to be briefly passed to the tile. DeleteStowedLoads on tile needs to be set to False, so that the load is not deleted. Logic to reparent the load must be done in OnProcess, not AMRArrived. ...
Posted By ⚙ Andrew Wu Sep 25, 2025 08:43:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Suryan, Did you remember to set DispatchInEnabled to True? I removed logic in your AMRGridManager that was setting DispatchInEnabled to False. -------------------------------------------
Posted By ⚙ Andrew Wu Sep 22, 2025 12:14:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi Suryan, The reason this happens is because setting DispatchInEnabled to False doesn't prevent incoming transfers from selecting that visual as a target. It only stops subsequent transfer events of that visual from happening until DispatchInEnabled is set to True again. This is global behaviour ...
Posted By ⚙ Andrew Wu Aug 05, 2025 07:32:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Version 18.0.2 of E3D 2025 will be releasing around the end of next week, my recommendation would be to update when it becomes available. If there are any stability/rendering issues, it is possible that the update may resolve them. -------------------------------------------
Posted By ⚙ Andrew Wu Aug 05, 2025 07:25:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Suryan, It looks like this happens because when there is more than one pending transfer, they are dispatched in a fixed order. In this case it happens to be for the left load, then the right load. This is not something that can be changed, and the order may vary depending on the situation. So ...