List of Contributions

W e i d a

Contact Details

W e i d a


My Content

1 to 20 of 38 total
Posted By W e i d a May 07, 2026 06:12:25 AM
Found In Library: Automation Control
Posted By W e i d a May 07, 2026 06:12:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, The studio 5000 shut down with popup error info: This is a problem for a long time.... Any help? Thanks. -------------------------------------------
Posted By W e i d a Nov 13, 2025 08:35:00 AM
Found In Egroup: Automation Control
\ view thread
Can Installing ME v16 fix these popups issues? -------------------------------------------
Posted By W e i d a Nov 13, 2025 08:28:00 AM
Found In Egroup: Automation Control
\ view thread
My laptop windows 11 updates are up to date. Jus installed FTview ME v15, and in control panel did a repair on FTview services platform 6.5. Reboot laptop and startup ME, open the project and get new popup: "The required SQL Server LocalDE instance is not found. Verify that SOL Server LocalDB is running ...
Posted By W e i d a Nov 13, 2025 07:38:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, laptop windows 10 upgraded to windows 11, removed FT view ME and re-installed FT view ME again, open the project with popup "Fail to load hmi server service". Can anybody help on this issue? Thanks. EDIT: moved to Automation Control community -FL -------------------------------------------
Posted By W e i d a Oct 14, 2025 07:05:05 AM
Found In Egroup: Automation Control
\ view thread
Version 30. I haven,t tried other versions yet. the program opened normal and get online with plc ok, but after a while it closed itself. -------------------------------------------
Posted By W e i d a Oct 14, 2025 06:31:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, Studio 5000 shut off itself after windows 10 ungraded to windows 11, any idea on this issue? -------------------------------------------
Posted By W e i d a Sep 29, 2025 08:27:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, Can FT view ME application convert to View designer files? How to convert? Thanks. EDIT: moved to Automation Control community -FL -------------------------------------------
Posted By W e i d a Jun 09, 2025 07:42:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, The dialogue property display not showing all the contents, See picture below, any help would be greatly appreciated. Thanks.
Posted By W e i d a May 27, 2025 07:33:00 AM
Found In Egroup: Automation Control
\ view thread
In each scan, the tag will be assigned a large value (which is the spike value coming from), then after this rung the tag will be assigned a calculated value. Even a fresh tag added on the last program rung, the spike will show up too. It is good to know the trend function/features. Thanks.
Posted By W e i d a Apr 28, 2025 06:45:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, When monitoring a real value tag, there are always some spikes show on the trends. Even clamping the tag value in the last plc rung, the spikes still come up. Each scan occasionally a large number will write to tag, but last rung clamping function seems not working. Does the trend will pick ...
Posted By W e i d a Apr 16, 2025 08:37:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I think this checkbox should be checked in offline program then download to plc, no drive parameters show up when it is running. I will try it later. Thanks.
Posted By W e i d a Apr 16, 2025 07:35:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Unfortunately, when monitoring the Axe motor, actualVelocity is -349, but currentFeedback is 0, no value. Any idea on this? See screenshot below.
Posted By W e i d a Apr 15, 2025 12:50:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Is .LoadObserverTorqueEstimate the one to monitor? Thanks.
Posted By W e i d a Mar 27, 2025 11:26:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, I am trying to understand the difference between the MAG and MDAC. Is MAG just for speed geared up with defined ratio only and no position synchronization? MDAC has the position synchronized function. Thanks.
Posted By W e i d a Mar 04, 2025 01:02:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I have trouble use this online tool, eg, add a motor. Can you share any help document or media? Thanks.
Posted By W e i d a Mar 03, 2025 06:51:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, Any gear servo motor available on AB brand? I couldn't find a catalogue. Thanks.
Posted By W e i d a Nov 25, 2024 08:44:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, There is a plc using produced and consumed tags, how to find out how many consumed and produced tags are used in the project? Thanks.
Posted By W e i d a Aug 21, 2024 11:57:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, eg, Drive1:O.FreqCommand = 1000 What Hz is this value referred to? Is the value reflecting the percentage of the max speed setup?
Posted By W e i d a Aug 15, 2024 01:35:00 PM
Found In Egroup: Networks
\ view thread
Tried from button, tools, menu, and right click the device, so far, nothing works.