List of Contributions

Robert Lightfoot

Contact Details

Robert Lightfoot


My Content

1 to 20 of 42 total
Posted By Robert Lightfoot Jan 16, 2026 06:56:00 AM
Found In Egroup: Automation Control
\ view thread
Thanks for the heads up, it made me double check. Looks like we moved our one V27 System to V28. That's why I've not seen your issue. For note I was trying to open an RSlogix 20 program when the issue of MSXML missing first raised it's head.
Posted By Robert Lightfoot Jan 15, 2026 10:45:00 AM
Found In Egroup: Automation Control
\ view thread
I am currently using all of the following: 1) RSLogix 5 Revision 10 2) RSLogix 500 Revision 12 3) RSLogix 5000 Revision 16.05 4) RSLogix 5000 Revision 17 5) RSLogix 5000 Revision 19 6) RSLogix 5000 Revision 20 7) Studio 5000 Revision 23 8) Studio 5000 Revision ...
Posted By Robert Lightfoot Jan 14, 2026 05:32:00 PM
Found In Egroup: Automation Control
\ view thread
If your IT department wants to upgrade to MSXML6 and tells you "Installing MSXML 6.0 will not affect existing applications that use MSXML 3.0 and MSXML 4.0. Version-independent" and "It won't break abything:" DO NOT TRUST THEM! It broke RSLinx and RSLogix5000 and Studio5000 on my systems. The ...
Posted By Robert Lightfoot Oct 21, 2025 05:52:00 PM
Found In Egroup: Advanced Software
\ view thread
Optional Work Around choose Customized Install and don't install FT Updater 4.30 agent if you have a working 4.20 on that node. -------------------------------------------
Posted By Robert Lightfoot Oct 21, 2025 01:49:00 PM
Found In Egroup: Advanced Software
\ view thread
10/21/2025 - Installing Factory Talk Studio Revision 16 upgrades previous versions of FT Updater to 4.30, Thus far FT Updater 4.30 Agent will not connect to FT updater 4.30 Server. Work Around was to downgrade to FT Updater 4.20 Agenr with 4.30 Server. Engineering at Rockwell is working ...
Posted By Robert Lightfoot Aug 20, 2025 06:50:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Thank you, Lesley, for explaining that MAJOR difference between 5400 NAT and the way the 9300-ENA and 1783-NATR work. I assume I missed it somewhere in the documentation, because external public devices never needed to be NAT mapped to vacant Private IP addresses with the 9300-ENA or 1783-NATR. ...
Posted By Robert Lightfoot Aug 19, 2025 10:55:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Please clarify something in your post for me? When trying to access the NAT translated device from the same VLAN on the public side, you will need to add a public to private translation as well for every 'public' device that needs to communicate with the private device. The Private Device ...
Posted By Robert Lightfoot Aug 14, 2025 01:20:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
The static NAT that you show is what we were trying to do and the 200.200.200.X addresses in your example don't arrive at the Cisco. The stratix 5400 doesn't translate them, even though it claims it does.
Posted By Robert Lightfoot Aug 13, 2025 11:43:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
This post is a bit of a rant and I apologize if I offend anyone, but I just finished spending six hours over three days on the phone with Rockwell "Experts" to learn the Stratix 5400 could not do NAT in the manner that the old reliable 1783-NATR does. If have achieved what I tried please share, I would ...
Posted By Robert Lightfoot Aug 19, 2024 10:17:00 AM
Found In Egroup: Automation Control
\ view thread
Ticket #4010758834 - Filed with Activations Team on this issue - 8/19/24 awaiting response.
Posted By Robert Lightfoot Aug 14, 2024 11:51:00 AM
Found In Egroup: Automation Control
\ view thread
Based on your video you are thinking that Updater will take you from Control Flash Plus 5.00 to 6.00. Is that what you're expecting? I am not an RA official commentor, but the purpose of Updater is to apply patches not to update between versions of a software package. That still has to be done ...
Posted By Robert Lightfoot Aug 14, 2024 11:26:00 AM
Found In Egroup: Automation Control
\ view thread
Which piece of software are you trying to update? Can you post a screenshot Like Philip and I did below.
Posted By Robert Lightfoot Aug 14, 2024 11:24:00 AM
Found In Egroup: Automation Control
\ view thread
Dear Philip: Makes me wonder the difference between your PC and mine at 4.10
Posted By Robert Lightfoot Aug 14, 2024 06:36:00 AM
Found In Egroup: Automation Control
\ view thread
It has worked for me from October of 23 until August of 24 when this bug popped up. Not that there haven't been issues. But keeping a dozen Rockwell Development PC patched it has been priceless.
Posted By Robert Lightfoot Aug 13, 2024 05:18:00 PM
Found In Egroup: Automation Control
\ view thread
The PCDC has a July 2024 Patch RollUp but Factory Talk updater over a dozen days into August, still shows the June 2024 Patch Roll Up as current and nothing in need of download. Also where is the promised 4.20 version??
Posted By Robert Lightfoot Apr 09, 2024 07:21:00 PM
Found In Egroup: Automation Control
\ view thread
Update - A rescan revealed patch did not deploy. Logs show no reason for install failure other than socket termination. RDP into agent and found free space below 6GB which means patch roll up could not be deployed. Freeing up space and patches deploy.
Posted By Robert Lightfoot Apr 09, 2024 03:57:00 PM
Found In Egroup: Automation Control
\ view thread
April 2024 Patch Tuesday - Factory Talk Updater still broken with respect to Connected Components Workbench Updates. ALSO NEW DEVELOPMENT - Patch Roll Up deployed to 10 Rockwell Development Stations and all came back "Patch Deploy Failed" ; click the "cancel" link as it's the only option and choose ...
Posted By Robert Lightfoot Mar 29, 2024 08:52:00 AM
Found In Egroup: Automation Control
\ view thread
Ticket #: 4010356400 - Was opened in November 2023 for this issue against 4.0 - closed because 4.10 was allegedly the fix. Ticket #: 4010506994 - Was opened in February 2024 for this issue against 4.10 - response "crickets" EDIT: fixed formatting -FL
Posted By Robert Lightfoot Mar 21, 2024 08:16:00 PM
Found In Egroup: Automation Control
\ view thread
It has been Five (5) months now and Factory Talk Updater V4.10 (still latests and greatest) says I need to patch my CCW13 and CCW21 systems, but fails when I attempt to do so and if I goto the PCDC and patch manually it does not acknowledge the patching. I know its free software, but it would be ...
Posted By Robert Lightfoot Feb 13, 2024 02:50:00 PM
Found In Egroup: Installation & Activation
\ view thread
Circling Back on PatchTuesday of Feb 2024 to confirm that FTUpdater V4.10 is now cleaning up after itself on the agents. Nice improvement!