List of Contributions

Rahul Vaze

Contact Details

Rahul Vaze


My Content

1 to 20 of 50+ total
Posted By Rahul Vaze May 31, 2026 04:36:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi , I am having a Stratix 5700 (Full Version) connected to a Control Logix PLC system . There are multiple Non Rockwell Devices ( VFD , RFID readers , Encoders) connected to this Switch . Now i wish to assign smart port roles for each of the port they are connected to . I am confused , as ...
Posted By Rahul Vaze May 20, 2026 11:03:00 AM
Found In Egroup: Automation Control
\ view thread
Hi , We have external hardware inputs from a Local field Station that we used for External Start and Stop . So we cant use it for External control
Posted By Rahul Vaze May 18, 2026 09:00:00 AM
Found In Egroup: Automation Control
\ view thread
Hi , Thanks for the reply . But we have a common PlantPax object(P_Motor , P_Valve) in the PLC . If HMI control is enabled then all the functions ( Program , Operator and External ) in PlantPax should be available and if SCADA control then the functions should be available through SCADA ,whereas ...
Posted By Rahul Vaze May 17, 2026 09:18:00 AM
Found In Egroup: Automation Control
\ view thread
We are having a FTVIEW ME system with PlantPax . In our system we also have a SCADA that uses FTVIEW SE that displays the same status as FTVIEW ME using PlantPax . Now Client wants to have Local/Remote Control facility ( using Pushbuttons connected to PLC) wherein if Remote PB is pressed the control ...
Posted By Rahul Vaze Jan 09, 2026 11:44:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi All , Is there any way for FTVIEW SE Data Report Generation in Excel . I am aware of FTVIEW SE logging in SQL but i cant figure out how to transfer the data from SQL into Excel using VBA and FTVIEW i.e A button click in SE page shall open the report in Excel . ------------------- ...
Posted By Rahul Vaze Oct 10, 2025 12:10:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Yes , it was solved . We introduced a signal isolator in between the Drive and Dgital Indicator .
Posted By Rahul Vaze Aug 18, 2025 07:55:00 AM
Found In Egroup: Advanced Software
\ view thread
Dear All , We are using FTVIEW 10 for one of our application and using Legacy Tag Alarms with logging enabled . When i click the HMI Tag Alarm Log Viewer properties to select the Log files i dont see it in proper format . It shows something like 2025 Liiqen 18-A , 2025 Liiqen 16-A as per ...
Posted By Rahul Vaze Jul 15, 2025 07:19:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi , We have a Powerflex 755 with add on I/O card and the analog output is connected to local digital indicator . It is observed that the Analog output from the Drive is not stable and the display indicator values fluctuates a lot . The Analog Output is configured correctly ( for Output Frequency ...
Posted By Rahul Vaze Jun 05, 2025 01:26:00 PM
Found In Egroup: Automation Control
\ view thread
Hi All , We are having a few E300 on a existing Devicnet network . Now we want to read trip Status from E300 over Device net via messaging . Is it possible ?? If so what could be class , attributes and Instances RV
Posted By Rahul Vaze Apr 03, 2025 11:05:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Thanks for the reply We tried to set it as mentioned but the response is very sluggish . Before atleast the drive response was fast but while lowering or even raising the drive with torque proven enabled the drive is jerking while running also . The time (1107 parameter number) was ...
Posted By Rahul Vaze Apr 03, 2025 11:01:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi , Yes we are using a PF755 I/O card to switch ON/OFF the mechanical brake . The Relay turns ON on the drive Running Status bit from the Drive
Posted By Rahul Vaze Apr 02, 2025 12:58:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi , We have PF755 controlling a Transfer car movement . The control mode is set to Induction SV and Accl and Decel Time are set to 2sec . The braking is dynamic . When the motor starts or stops then we have always a Jerk . We tried to elimnate it using longer accel and decel time but then ...
Posted By Rahul Vaze Mar 05, 2025 10:38:00 AM
Found In Egroup: Automation Control
\ view thread
Hi All , We are using a Control Logix L83ES with V35 . We have a lot of SFC in it for various machine . Is there any way to obtain the Status of the SFC routine i.e whether the routine is paused or Running . I am aware that we put a SFC in either a Pause state or Running State , but is it ...
Posted By Rahul Vaze Feb 09, 2025 05:39:00 AM
Found In Egroup: Automation Control
\ view thread
Hi All , I am facing a peculiar issue with one of the outputs of 5094-OB8 . Whenever i force the output to ON from the controller , the output LED of the particular channel keeps blinking ( Yellow light ON/OFF ) . This is happening for only one particular output whereas all other outputs ...
Posted By Rahul Vaze Jan 25, 2025 11:18:00 PM
Found In Egroup: Automation Control
\ view thread
Hi All , I have a query regarding SFC execute and Pause in SFC State Instruction. I am aware that by using SFR i can reset the SFC to the required state . But i am confused regarding SFC execute and Pause. Do i need to enable the execute only one time and the SFC executes continously ...
Posted By Rahul Vaze Jan 05, 2025 03:21:00 AM
Found In Egroup: Automation Control
\ view thread
Is it possible that in IB16S i dont use the SA+ power Row i.e Test Output Points will be configured as None . Field Emergency Stops will be connected to the IB16s inputs . They will be from a common Power Supply and the Gnd of the Power Supply will be connected to the IB16S SA-
Posted By Rahul Vaze Dec 30, 2024 12:24:00 AM
Found In Egroup: Automation Control
\ view thread
Hi , I am using a Safety PLC 1756-L83ES . I have emergency stop over the field areas . I am using DCS instruction for it . Everything works fine , however when i restart the PLC system , i need to Reset each and every emergency in the field and then press Reset for the Safety System to be ...
Posted By Rahul Vaze Dec 22, 2024 01:20:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi , I am using a Powerflex 755 to control the speed of the Lifting Table UP/Dwn . The Table is driven by Motor that has a brake which is turned ON when the drive is ON (using the Relay Out of PF755 . Relay Out is turned ON when the Drive Running bit of the Drive Status is Active ) . Now when i ...
Posted By Rahul Vaze Dec 22, 2024 12:24:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi , But i am not using giving a seprate Stop command . I am just using a Command Run command
Posted By Rahul Vaze Dec 22, 2024 12:21:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Yes the jumpers are set accordingly . Still i cant have Safe Torque ( with Hardware and Ethernet) and i am getting fault 104 as mentioned in the page 75 of the above mentioned manual . Any suggestions