List of Contributions

STEVE BINKS

Contact Details

STEVE BINKS


My Content

1 to 20 of 26 total
Posted By STEVE BINKS May 26, 2026 09:05:00 AM
Found In Egroup: Automation Control
\ view thread
I have a recent application with PVP7 standard & L320ER@v30 It has worked fine for a couple of weeks, but now refuses to print from PV ( via ethernet ) and shows numeric tags as ?????? on some screens while showing the correct value for the same tags on another screen and not displaying same tags ...
Posted By STEVE BINKS Apr 29, 2026 08:43:00 AM
Found In Egroup: Automation Control
\ view thread
Your RSLogix5000 is the software you use for all the tasks your list, however it needs to be the same (major) version as the PLC you are connecting to i.e. Logix v20 for 1756 v20. With RSLinx you should be able to connect your laptop ethernet port to 1756 ethernet card or USB to PLC USB port, this will ...
Posted By STEVE BINKS Mar 10, 2025 03:39:00 AM
Found In Egroup: Installation & Activation
\ view thread
I have 2 W10 VMs, a network one which can load V13 programs, and a local one which tries to run EVmove (and failing because its not a 64 bit program). Both machines have the same licenses, a legacy one which I understand uses Flexera not codemeter Use CodeMeter First checkbox is cleared ...
Posted By STEVE BINKS Jan 31, 2025 08:38:00 AM
Found In Egroup: Automation Control
\ view thread
There is a processor HMI faceplate available in sample code
Posted By STEVE BINKS Jan 31, 2025 08:27:00 AM
Found In Egroup: Automation Control
\ view thread
Try Unlatching the channel Underrange bit every scan
Posted By STEVE BINKS Jan 23, 2025 05:59:00 AM
Found In Egroup: Automation Control
\ view thread
Is there, maybe, a master reset that can be done on the processor without turning it into a brick? Yes there is a small hole under the run switch where you can insert a paperclip while powering up, this clears the memory - useful on a safety PLC when you can't remember the password ;0
Posted By STEVE BINKS Dec 05, 2024 06:23:00 AM
Found In Egroup: Automation Control
\ view thread
FW v1.1 is a virgin device, previously unused SO flash it in a bench setup as above, if you can use a Ethernet card like EN2T with a USB port then use that
Posted By STEVE BINKS Dec 02, 2024 07:58:00 AM
Found In Egroup: Automation Control
\ view thread
Put the other PLC in each others IO tree at the bottom, with their IP addresses, then configure your produced tags with 1 consumer, then your consumed tags with the producer selected from the IO tree, make sure both PLC are set to same task rates. are you sending safety tags?
Posted By STEVE BINKS Dec 02, 2024 07:47:00 AM
Found In Egroup: Automation Control
\ view thread
I can hear tech support saying " have you installed the latest version?" I have done this on 20.05 but NOT online Steve
Posted By STEVE BINKS Dec 02, 2024 07:41:00 AM
Found In Egroup: Automation Control
\ view thread
Your FPD likely provides Emergency stopped power to the output cards so that all points on those cards will be off for an E-stop. So you should put your input card before the FPD and re-map the 2 output cards Steve
Posted By STEVE BINKS Dec 02, 2024 07:37:00 AM
Found In Egroup: Automation Control
\ view thread
In Global Connections - Display, you can find the Remote Display Number to display the chart object page, then Remote Display Print to print the page on view Steve
Posted By STEVE BINKS Dec 02, 2024 01:02:00 AM
Found In Egroup: Automation Control
\ view thread
Logix v33 on W10, added EDS files for multiple PLX32-EIP modbus cards, now when selecting my card I get error 8612-80043A12 Rebooting makes no difference, help file is no help, Knowledgebase seems to have no entry for this error Does anyone have any tips Steve
Posted By STEVE BINKS Nov 07, 2024 07:24:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Ryan I would normally do that for reading current or power, that change all the time, but not for a value that should be constant. Which is why I followed the original messaging technique, it only talks to each inverter once every 12 seconds instead of very 200ms Is there ...
Posted By STEVE BINKS Nov 07, 2024 04:30:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi All, upgrading several (12) PF40 to PF525, trying to re-use the parameter read message for Max Speed but failing with error 16#0001 ext code 16#0001_0315, obviously changed the parameter field to 44. In communication tab I see the correct drive name passed in from an array e.g. $01$02$12$p192.168.2.15 ...
Posted By STEVE BINKS Mar 20, 2024 02:12:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I have a PF525 7.5HP 5.5KW 460V which thinks its a 460V 1.0HP After setting par#53 to 3 (Power Reset) its still the same After flashing v7.001 ( which it originally came with) it thinks it is 600V 2.0HP After setting par#53 to 3 (Power Reset) its back to 460V 1.0HP Is there anything ...
Posted By STEVE BINKS Jan 29, 2024 03:25:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Sarille This is a massive problem for lots of us, Studio5000 loses a temporary file it created and I wish Rockwell could get to the bottom of it Registry tuning, viruses, UAC (User Access Control) and various other reasons have been blamed It has even been suggested that I uninstall ...
Posted By STEVE BINKS Jan 18, 2024 09:33:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
And if I cannot access the motor rating plate so don't know poles or rpm, what effect will this have on the motor e.g use the default 2 poles for a 4 poles motor ------------------------------ STEVE BINKS ------------------------------
Posted By STEVE BINKS Jan 17, 2024 08:27:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I have a motor that is unreachable without the scaffolding that it was installed with, so unsure of exact details on rating plate. Do the rpm and number of poles parameters do anything critical other than provide rpm readout? PF525 but also PF753/755 for future reference ------------------------------ ...
Posted By STEVE BINKS Dec 19, 2023 06:06:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Mica Thanks for the link, but damn Rockwell knows how to charge, that card is 3x the price of the standard STO card so that totally negates the saving of 2 safety outputs So unless its the only drive in the cabinet and I can save on AENT card too, then its not a great saving After working ...