|
Hello TJ, but I can't get one drive to start when it only has 50% actual load Below 16Hz, the drive is peaking at 150% torque (limited) on P4, and it is stalling and keeps tripping, even though the real mechanical torque is only 50% Once it has run above 16Hz, the torque reading on P4 drops to 50% ...
|