List of Contributions

Kakkerlak

Contact Details

Kakkerlak


My Content

1 to 20 of 22 total
Posted By Kakkerlak Jul 05, 2026 09:31:19 PM
Found In Egroup: Automation Control
\ view thread
Go ahead and start it up while running a stopwatch, and note the time it takes for each stage to complete, especially time time after the application starting notice appears. Create a dummy program with no tags connected and just one screen. See how long that takes to start up. My speculation is that ...
Posted By Kakkerlak Jun 25, 2026 08:22:00 AM
Found In Egroup: Automation Control
\ view thread
Why did you replace the 20-COMM-D ? The most likely explanation is that you didn't re-configure the 20-COMM-D with the appropriate datalinks and connection size, which would result in an Error 77 code on the scanner. Do you have access to any notes or documents or similarly-configured drives so ...
Posted By Kakkerlak May 01, 2026 02:01:00 PM
Found In Egroup: Automation Control
\ view thread
Can you get to the configuration menu screen that describes the main board and daughtercard hardware strings and revisions ? You can get that error if the daughtercard is mis-identifying itself to the main board, even for the four variants of DH485 comms daughtercards. Or if someone "refurbished" ...
Posted By Kakkerlak Mar 17, 2026 12:40:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
If you were asking for Modbus protocol experience, then you should not have specifically asked for DH-485 experience with an RS-485 wireless bridge. If you already knew better, then you should have stated so. -------------------------------------------
Posted By Kakkerlak Mar 16, 2026 10:47:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Data Highway 485 has some very tight timing requirements for token-passing. While asynchronous protocols like DF1 or Modbus RTU can accept some variation and delays, DH485 cannot. You will not find any successful DH485 over radio applications.
Posted By Kakkerlak Dec 15, 2025 12:03:00 AM
Found In Egroup: Automation Control
\ view thread
The 1746-IB16 was a very popular 24V sinking DC input module for the SLC-500 modular hardware system. I was one of the last modules to go out of production, presumably because of its high popularity: RA stopped making them at the end of 2021. You can look up the lifecycle status of most RA products: ...
Posted By Kakkerlak Aug 23, 2025 02:50:00 AM
Found In Egroup: Legacy
\ view thread
That "CP3" cable is not a DH485 protocol converter. It will support DF1 protocols, or Modbus or ASCI or other protocols that don't use careful timing in their token rotation like DH485 does. It can connect to the Channel 0 port of an SLC-5/03 controller if that port is set up for any protocol except ...
Posted By Kakkerlak Aug 21, 2025 04:16:00 PM
Found In Egroup: Legacy
\ view thread
There is a third-party alternative sold by PLCCable.com. While Rockwell Automation does not support that device, it has a very good reputation for compatibility. https://www.plccable.com/allen-bradley-1747-uic-usb-to-dh485-usb-version-1747-pic-slc500/ -------------------------------------------
Posted By Kakkerlak Aug 05, 2025 01:44:00 AM
Found In Egroup: Legacy
\ view thread
Do you think that the PanelView used any of the discrete I/O table for addressable memory, or did it just use Block Transfers ? I agree that taking out the Block Transfers and just addressing the PLC-5 Data Tables that they use as their sources and destination is the most straightforward method. Deleting ...
Posted By Kakkerlak Jul 30, 2025 12:51:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
You will find the Optix comms drivers complaining a little about not being able to get extended tag properties from v20 controllers, but it will definitely work. I do most of my testing with 1756-L61 v20. -------------------------------------------
Posted By Kakkerlak Jul 19, 2025 06:21:00 PM
Found In Egroup: Automation Control
\ view thread
I realize this post is several weeks old, but I wanted to post a reply. The "trip Status" should already be part of the Input Assembly that is polled by the DeviceNet scanner. The first two 16-bit words in the simplest Instance 131 input assembly contain Device Status 0 and Device Status 1, which ...
Posted By Kakkerlak Jun 24, 2025 01:06:00 AM
Found In Egroup: Advanced Software
\ view thread
Try adding "/Backplane/0" to the Route field. Even though the Ethernet port is physically built into the 1769-L35E enclosure instead of being a separate slot-mounted device, it is more like a virtual backplane with the controller in Slot 0.
Posted By Kakkerlak May 20, 2025 11:02:00 PM
Found In Egroup: Advanced Software
\ view thread
I would start by seeing if RSLinx browsing is the only protocol effected. Have that user try other kinds of connectivity, like good old ICMP PING at the Command prompt, and HTTP to the 1756-ENBT's address in a web browser. Also, try Windows Powershell's test-netconnection command, which allows ...
Posted By Kakkerlak Apr 30, 2025 06:46:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
My understanding is that FTOptix includes embedded instances of SQLite (what they just call "embedded") and InfluxDB that don't require separate installation or management. If you want to use an external InfluxDB server, on the local PC or on a separate machine, you need to install and configure it yourself. ...
Posted By Kakkerlak Apr 29, 2025 09:46:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I think it's worth asking your customer what their experience is with historians, and how they intend to analyze and store this data. Just logging data for a trend isn't really getting into the compression and analysis features that real industrial historian packages have. Don't expect to use the ...
Posted By Kakkerlak Apr 25, 2025 07:00:00 PM
Found In Egroup: Advanced Software
\ view thread
I realize this post is many weeks old, but I wanted to be sure it got at least a shot at an answer. FTView ME version 7 and higher support up to 1 million records in the internal data log. Previously, the limit was 300,000. If you were logging just one tag, every 1 second, that would run for 11.57 ...
Posted By Kakkerlak Apr 23, 2025 03:31:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
(not-OP again) Thank you for that thoughtful and informative answer. It's especially helpful to get an explanation of what the ComboBox does under the hood and be reminded that there are visibility and sorting features, which makes a simple "which element was selected, numbered from the top" value ...
Posted By Kakkerlak Apr 23, 2025 12:21:00 PM
Found In Egroup: Automation Control
\ view thread
Describe the terminals in a little more detail. Ideally, post the actual part number. PanelView Plus (2711P) wasn't released until version 3.0, back in 2003 or so. PanelView Standard flatscreen terminals were up to v4.x by the end of their life. I'm only familiar with version 1.x for the PanelView ...
Posted By Kakkerlak Apr 23, 2025 12:05:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Also: thank you for explaining how the (Item) alias works: it's an alias for the selected element of the ComboBox drop-down, rather than a reference to the ComboBox itself.
Posted By Kakkerlak Apr 23, 2025 11:51:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I was participating in this discussion on another forum, and I'm going to poke my nose in here. I am not the original poster, just a FTOptix novice. I think that what makes this application unusual is that the desired labels for the ComboBox are in a STRING[x] array tag in a ControlLogix, not in a ...