List of Contributions

Peter - PSA1

Contact Details

Peter - PSA1


My Content

1 to 20 of 50+ total
Posted By Peter - PSA1 Apr 10, 2026 02:10:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Philip, Thank you but I know what a DLR is. I did do a quick search and found..."A Dynamic Link Library (DLL) is a type of file in Microsoft Windows operating systems that contains a collection of shared code, data, and resources (such as icons or fonts) that multiple programs can use simultaneously. ...
Posted By Peter - PSA1 Apr 09, 2026 09:27:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
I have been editing prints for a customer and the end user (EU) requires the use of a 1783-HMS16T4CGN. Yes, it is a discontinued part number but they have updated their Approved Components Appendix and it is the only 20 port switch that is approved. They (EU) reviewed my first revision and suggested ...
Posted By Peter - PSA1 Mar 13, 2026 06:28:00 AM
Found In Egroup: General Discussions
\ view thread
Per the notes in the app... Current Program Updater Information: This application provides you with the ability to continuously look for updates on various Rockwell Automation applications you have installed on your computer. Once you install an application that supports this functionality, you ...
Posted By Peter - PSA1 Mar 08, 2026 10:56:00 AM
Found In Egroup: Automation Control
\ view thread
Dex, I would be using a new Micro850 (2080-L50E-48AWB). I would still need to do the PCCC mapping, correct? It would not be plug and play as a new PanelView800 would be, correct? ------------------------------ Peter Sherick P Squared Automation, ltd. ------------------------ ...
Posted By Peter - PSA1 Mar 07, 2026 01:10:00 PM
Found In Egroup: Automation Control
\ view thread
Thank you. I did not want to assume anything. I have used Series B on several projects but not Series A. ------------------------------ Peter Sherick P Squared Automation, ltd. ------------------------------
Posted By Peter - PSA1 Mar 07, 2026 11:06:00 AM
Found In Egroup: Automation Control
\ view thread
I am quoting a PLC update from a Micrologix 1200 to a Micro850. The customer currently has the HMI in the subject. Could someone please confirm that the Micor800 series PLC's can communicate with the older PanelView 800 HMI's? ------------------------------ Peter Sherick P Squared Automation, ...
Posted By Peter - PSA1 Jan 19, 2026 08:51:00 AM
Found In Egroup: Automation Control
\ view thread
I am considering my Rockwell HMI options. I have used the PanelView 800 series on past projects. To be honest, not bad for for an 'entry level' HMI from Rockwell. I am trying to save myself and my client some money and programming time for the initial cost of the project but also year over year investment ...
Posted By Peter - PSA1 Jan 06, 2026 04:11:00 AM
Found In Egroup: Automation Control
\ view thread
I threw some stuff into Proposal Works just to get an idea of status, availability, and cost (list price)... 1734-Point IO are all 'Active'. Communications module 1734-AENTR has a lead time of 29 days. (2) 1734-IB8's and (2) 1734-OB8's have a 1-5 day lead. Cost: +/- $1500. Fewer IO/module and the ...
Posted By Peter - PSA1 Dec 11, 2025 07:07:00 PM
Found In Egroup: Automation Control
\ view thread
I am designing a 5069-L330ERMS rack with multiple Safe IO 24V Cards and Standard 24V Cards. I have to incorporate (1) 5069-IA16 and (2) 5069-IF8 cards. I believe I need a 5069-FPD in the previous slot before the 5069-IA16. Do I need another FPD after the IA16 for the (2) IF8's? The prints for the ...
Posted By Peter - PSA1 Dec 05, 2025 07:30:00 PM
Found In Egroup: Automation Control
\ view thread
Funny enough that is the exact same table my local distributor supplied me for the same question. If the 249mA is all inclusive, I'll be okay. If not and I can't get a straight answer then I need to find an alternate. ------------------------------ Peter Sherick P Squared Automation, ltd. -- ...
Posted By Peter - PSA1 Dec 05, 2025 07:20:00 PM
Found In Egroup: Automation Control
\ view thread
GLaDOS, That is the same table as I found. That's the load for the Beacon but nothing for the Audible Alarm. Thanks for looking! ------------------------------ Peter Sherick P Squared Automation, ltd. ------------------------------
Posted By Peter - PSA1 Dec 02, 2025 06:12:00 PM
Found In Egroup: Automation Control
\ view thread
I have looked through a handful of resources on this Low-Profile Audible Alarm Base and I cannot find the Max Current for the Audible Alarm. I have found the Max Current for the Steady On Beacon model I have specified for my project. No luck with this audible base. Please help. ------------------------------ ...
Posted By Peter - PSA1 Jun 17, 2025 12:19:00 PM
Found In Egroup: Automation Control
\ view thread
I received an answer from Mike at TechConnect: All 3 Rockwell 5069 Series Digital Input Modules are SINKING Input Modules and thus cannot be used with NPN Sensors. Thanks for the sanity check. ------------------------------ Peter Sherick P Squared Automation, ltd. ---------------------- ...
Posted By Peter - PSA1 Jun 17, 2025 10:47:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, I have a 5069-IB16 (Slot 5) not seeing inputs. All NPN Sensors are being used on this card. When a sensor is ON (made), I see +24V DC. When the same sensor is OFF, I see +19V DC. When uncoupled from the Module, ON = +24V DC. OFF = 0V DC. (This tells me the field wiring is correct.) ...
Posted By Peter - PSA1 Jun 10, 2025 03:55:00 PM
Found In Egroup: Automation Control
\ view thread
Hello, I am working through bringing a small system online. I am receiving the fault code in a CROUT instruction. Logic: Alarm #: I will browse the knowledge base but I wanted to throw it up here to see what sticks. Card is configured Bipolar. Feedback 1 and 2 are signals ...
Posted By Peter - PSA1 Jun 09, 2025 12:27:00 PM
Found In Egroup: Automation Control
\ view thread
QA49239 - Solution 3 worked. PLC is now flashed and program installed. ------------------------------ Peter Sherick P Squared Automation, ltd. ------------------------------
Posted By Peter - PSA1 Jun 09, 2025 10:50:00 AM
Found In Egroup: Automation Control
\ view thread
Fuzzy, Yes, the download appears in the Manage Firmware list. RA had me switch to ControlFLASH. Now, I'm fighting through their fixes for the 'User has no access...' error. Working through the tech note now. ------------------------------ Peter Sherick P Squared Automation, ltd. ------- ...
Posted By Peter - PSA1 Jun 09, 2025 09:04:00 AM
Found In Egroup: Automation Control
\ view thread
I'm having trouble flashing this PLC... Downloaded the firmware yet I cannot flash the device. Stays grayed out/unavailable. ------------------------------ Peter Sherick P Squared Automation, ltd. ------------------------------
Posted By Peter - PSA1 May 09, 2025 06:45:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, Since you are using Latch/Unlatch bits, there is no need to 'Latch' you 'Motor_Start_Request' with itself. (Unnecessary redundancy). I also suggest moving your one-shot inside of your branches. This will allow Floats 1 & 2 to trigger (pulse) your start request when Float 2 Closes. With ...
Posted By Peter - PSA1 Mar 24, 2025 07:27:00 AM
Found In Egroup: Automation Control
\ view thread
I do not have the hardware to test my screen layouts. I am establishing my standard global items for each individual screen (similar to PV+ applications). With the 800 series there are no 'global objects'. My question is this... Is there a way of viewing/testing screens without the actual hardware? ...